cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMX MATLAB Hardware Setup

JakeBrake101
Visitor

Hello team!!

 

Perhaps this issue is solved somewhere, just want to be pointed on the right direction.

Recently I got two NUCLEO boards (G474 & F334) and wnated to make a fast prototype on them, the first thing I did is the simple "blinky" prog to check if all were fine.

 

As I am fast prototyping, I use SIMULINk to generate the necesary file to do the job.

Now, I followed the instructions to registered to use with MATLAB and Simulink, downloaded the file in ST required version 6.4.0) and after installing the version is nor recognized (see first attachement).

The STM32CubeMX. exe works as intended, so no issue there~

 

I checked the .exe  file properties and indeed it has File version 4.1.0.0 (second attachement)!

 

Now, how I can indicate that the version is correct, get the real file with v6.4.0 or how to modify the version in the .exe file to be recognized.

 

And yes, I know that MATLAB has to ask for more recent file but let's be constructive and find the solution.

 

Thank you.

 

 

 

0 REPLIES 0