cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMX Feature Requests

qwer.asdf
Senior
Posted on May 19, 2015 at 12:13

Can this be a semi-official feature-request thread for STM32CubeMX?

1. Show somewhere the essential parameters of the currently selected MCU (like flash size, RAM size, speed, etc.)

2. Add more filters when selecting MCU. I needed a HW Crypto filter not so long ago for example.

3. Add an option to change the MCU if the used peripherals are compatible with the target MCU (it can be wizard-style so the user can help the algorithm to solve conflicts).

4. Add an option for creating custom boards in the Boards list

5. This may sound silly for ST who are not used to open source movement, but why not open up the CubeMX and move its development to GitHub? These days even

https://github.com/microsoft

are making

http://blogs.msdn.com/b/dotnet/archive/2014/11/12/net-core-is-open-source.aspx

towards open source. I don't think there is know-how technology in CubeMX and ST is a hardware company not software, so it should be safe to open source it and you will be amazed how much quality feedback and pull requests you will get back from the community for free of charge.

#cube
This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
stm32cube-t
ST Employee
Posted on May 25, 2015 at 19:06

Hello,

Thank you for your requests. Please find some feedback below:

1. Show somewhere the essential parameters of the currently selected MCU (like flash size, RAM size, speed, etc.)

-> enhancement will be raised.

2. Add more filters when selecting MCU. I needed a HW Crypto filter not so long ago for example.

-> enhancement will be raised.

3. Add an option to change the MCU if the used peripherals are compatible with the target MCU (it can be wizard-style so the user can help the algorithm to solve conflicts).

-> already part of our enhancement list.

4. Add an option for creating custom boards in the Boards list

-> enhancement will be raised.

Regarding open source development, this is not yet considered.

Best regards

qwer.asdf
Senior
Posted on May 27, 2015 at 16:01

Thank you for your time and consideration.

Svenn Dahlstrom
Associate III
Posted on May 28, 2015 at 10:22

Here is an other request for the STM32CubeMX.

1. Be able to add an mail queue in Freertos.

stm32cube-t
ST Employee
Posted on March 22, 2016 at 19:38

Dear user,

Note most of your requests have been implemented (user boards not yet).

Best regards