cancel
Showing results for 
Search instead for 
Did you mean: 

stm32cubeide fatfs f_close FS_DISK_ERR

MSilv.1
Associate II

I have a board with stm32f407zgt6. I'm using freertos and fatfs. The board has a connection for an SDCARD, I'm using a 4GB SDCARD with fat32.

For reading, F_open, f_read, f_close, everything works. When I use it to write, f_close takes a long time and returns FS_DISK_ERR.

What do you need, files, the .ioc, the sources, no problem, to help me find the problem? I tried to configure it as correctly as possible, but I think I left something behind.

The write process it's in the file ESP8266_HALL.cpp, this file I put in the body of the post, because the forum did not accept the file for a reason that I did not understand, but I will not fight with the forum, I really want help.

Thank you very much.

PS: f_write return the correct amount of bytes written, with what I ordered to be written. the file, after the f_close error, has 0 bytes on the disk. This happens both for already existing files and for new files

 

 

/*
 * ESP8266_HAL.c
 *
 *  Created on: Apr 14, 2020
 *      Author: Controllerstech
 */


#include "UartRingbuffer_multi.h"
#include "ESP8266_HAL.h"
#include "stdio.h"
#include "string.h"
#include "stdlib.h"
#include "fatfs.h"
#include "MCUFRIEND_kbv.h"

extern UART_HandleTypeDef huart1;
extern UART_HandleTypeDef huart2;

extern TIM_HandleTypeDef htim11;
extern TIM_HandleTypeDef htim13;

#define wifi_uart &huart1
#define pc_uart &huart2

#define FORWARD  1
#define BACKWARD 2
#define BRAKE    3
#define RELEASE  4

extern MCUFRIEND_kbv tft;

char buffer[20];

char *Basic_inclusion = (char*)"<!DOCTYPE html> <html>\n<head><meta name=\"viewport\"\
		content=\"width=device-width, initial-scale=1.0, user-scalable=no\">\n\
		<title>MMSJ800</title>\n<style>html { font-family: Helvetica; \
		display: inline-block; margin: 0px auto; text-align: center;}\n\
		body{margin-top: 50px;} h1 {color: #444444;margin: 50px auto 30px;}\
		h3 {color: #444444;margin-bottom: 50px;}\n.p {font-size: 14px;color: #888;margin-bottom: 10px;}\n\
		</style>\n</head>\n<body>\n<h1>MMSJ800</h1>\n";

char *Terminate = (char*)"</body></html>";



/*****************************************************************************************************************************************/

//--------------------------------------------------------------------------------
char ESP_Init (char *SSID, char *PASSWD)
{
	char data[80];
	Ringbuf_init();
	char vError = 0;

	Uart_sendstring("\r\n\r\nStarting...\r\n", pc_uart);

	tft.print(".");
	Uart_sendstring("AT+RST\r\n", wifi_uart);
	Uart_sendstring("RESETTING.", pc_uart);
	for (int i=0; i<5; i++)
	{
		HAL_Delay(1000);
	}

	/********* AT **********/
	Uart_flush(wifi_uart);
	Uart_sendstring("AT\r\n", wifi_uart);
	while(1)
	{
		if (Wait_for((char*)"OK\r\n", wifi_uart))
		{
			Uart_sendstring("OK\r\n", pc_uart);
			break;
		}
		else if (Wait_for((char*)"Error\r\n", wifi_uart))
		{
			Uart_sendstring("Error\r\n", pc_uart);
			vError = 1;
			break;
		}
	}
	if (vError)
	{
		tft.print("...Error!!!");
		Uart_sendstring("\r\nAT---->ERROR\r\n", pc_uart);
		return -1;
	}

	tft.print(".");
	Uart_sendstring("\r\nAT---->OK\r\n", pc_uart);

//	tft.fillScreen(TFT_BLACK);
//	tft.setCursor(0, 16);

	/********* AT+CWJAP="SSID","PASSWD" **********/
	Uart_flush(wifi_uart);
	Uart_sendstring("connecting... to the provided AP\r\n", pc_uart);
	sprintf (data, "AT+CWJAP=\"%s\",\"%s\"\r\n", SSID, PASSWD);
	Uart_sendstring(data, wifi_uart);
	HAL_Delay(3000);
	while(1)
	{
		if (Wait_for((char*)"OK\r\n", wifi_uart))
			break;
		else if (Wait_for((char*)"Error\r\n", wifi_uart))
		{
			vError = 1;
			break;
		}
	}
	if (vError)
	{
		Uart_sendstring("Error Connecting\r\n", pc_uart);
		return -1;
	}

	tft.println(".");
	sprintf (data, "Connected to \"%s\"", SSID);
	tft.print(data);
	Uart_sendstring(data,pc_uart);
	Uart_sendstring("\r\n",pc_uart);

	/********* AT+CWMODE=1 **********/
	Uart_flush(wifi_uart);
	Uart_sendstring("AT+CWMODE=1\r\n", wifi_uart);
	while(1)
	{
		if (Wait_for((char*)"OK\r\n", wifi_uart))
			break;
		else if (Wait_for((char*)"Error\r\n", wifi_uart))
		{
			vError = 1;
			break;
		}
	}
	if (vError)
	{
		Uart_sendstring("CW MODE---->ERROR\r\n", pc_uart);
		return -1;
	}

	tft.print(".");
	Uart_sendstring("CW MODE---->OK\r\n", pc_uart);

	/********* AT+CIFSR **********/
/*	Uart_flush(wifi_uart);
	Uart_sendstring("AT+CIFSR\r\n", wifi_uart);
	HAL_Delay(3000);
	while(1)
	{
		if (Wait_for((char*)"CIFSR:STAIP,\"", wifi_uart))
			break;
		else if (Wait_for((char*)"Error\r\n", wifi_uart))
		{
			vError = 1;
			break;
		}
	}
	if (vError)
	{
		Uart_sendstring("CIFSR---->ERROR\r\n", pc_uart);
		return -1;
	}
	while (!(Copy_upto((char*)"\"",buffer, wifi_uart)));
	while(1)
	{
		if (Wait_for((char*)"OK\r\n", wifi_uart))
			break;
		else if (Wait_for((char*)"Error\r\n", wifi_uart))
		{
			vError = 1;
			break;
		}
	}
	if (vError)
	{
		Uart_sendstring("Error Getting IP\r\n", pc_uart);
		return -1;
	}

	int len = strlen (buffer);
	buffer[len-1] = '\0';
	sprintf (data, "IP ADDR: %s\r\n", buffer);
	Uart_sendstring(data, pc_uart);*/

	/********* AT+CIPSTA **********/
	Uart_flush(wifi_uart);
	Uart_sendstring("Setting Static IP...\r\n", pc_uart);
	sprintf (data, "AT+CIPSTA=\"192.168.0.67\",\"192.168.0.1\",\"255.255.255.0\"\r\n");
	Uart_sendstring(data, wifi_uart);
	HAL_Delay(3000);
	while(1)
	{
		if (Wait_for((char*)"OK\r\n", wifi_uart))
			break;
		else if (Wait_for((char*)"Error\r\n", wifi_uart))
		{
			vError = 1;
			break;
		}
	}
	if (vError)
	{
		Uart_sendstring("Error Connecting\r\n", pc_uart);
		return -1;
	}

	tft.print(".");
	sprintf (data, "Static IP set to 192.168.0.67\r\n");
	Uart_sendstring(data,pc_uart);

	/********* AT+CIPMUX **********/
	Uart_flush(wifi_uart);
	Uart_sendstring("AT+CIPMUX=1\r\n", wifi_uart);
	while(1)
	{
		if (Wait_for((char*)"OK\r\n", wifi_uart))
			break;
		else if (Wait_for((char*)"Error\r\n", wifi_uart))
		{
			vError = 1;
			break;
		}
	}
	if (vError)
	{
		Uart_sendstring("CIPMUX---->ERROR\r\n", pc_uart);
		return -1;
	}

	tft.print(".");
	Uart_sendstring("CIPMUX---->OK\r\n", pc_uart);

	/********* AT+CIPSERVER **********/
	Uart_flush(wifi_uart);
	Uart_sendstring("AT+CIPSERVER=1,80\r\n", wifi_uart);
	while(1)
	{
		if (Wait_for((char*)"OK\r\n", wifi_uart))
			break;
		else if (Wait_for((char*)"Error\r\n", wifi_uart))
		{
			vError = 1;
			break;
		}
	}
	if (vError)
	{
		Uart_sendstring("CIPSERVER---->ERROR\r\n", pc_uart);
		return -1;
	}

	tft.println(".");
	tft.print(data);
	Uart_sendstring("CIPSERVER---->OK\r\n", pc_uart);
	Uart_sendstring("Now Connect to the IP ADRESS\r\n", pc_uart);

	return 0;
}

//--------------------------------------------------------------------------------
int Server_Send (char *str, int Link_ID)
{
	int len = strlen (str);
	char data[80];

	sprintf (data, "AT+CIPSEND=%d,%d\r\n", Link_ID, len);
	Uart_sendstring(data, wifi_uart);
	while (!(Wait_for((char*)">", wifi_uart)));
	Uart_sendstring (str, wifi_uart);
	while (!(Wait_for((char*)"SEND OK", wifi_uart)));
	sprintf (data, "AT+CIPCLOSE=5\r\n");
	Uart_sendstring(data, wifi_uart);
	while (!(Wait_for((char*)"OK\r\n", wifi_uart)));
	return 1;
}

//--------------------------------------------------------------------------------
void Server_Handle (char *str, char *resphttpcode, int Link_ID)
{
	int len = strlen (str);
	char response[200];

    sprintf(response,
        "HTTP/1.1 %s\r\n"
        "Content-Type: text/plain\r\n"
        "Content-Length: %d\r\n"
        "Connection: close\r\n"
        "\r\n"
        "%s", resphttpcode, len, str);

	Server_Send(response, Link_ID);
}

//--------------------------------------------------------------------------------
void Server_Start (void)
{
	char buftocopyinto[512] = {0};
	char Link_ID, cRec;
	int ix, indx;
	unsigned int postLen, lenSave, vhead, vtail, timeout;
	char* vPosIni;
	char data[320];
	char slen[10];
	char filename[12];
	FIL basicFile;
	FRESULT res;

	while (!(Get_after((char*)"+IPD,", 1, &Link_ID, wifi_uart)));

	Link_ID -= 48;

	while (!(Copy_upto((char*)"\r\n\r\n", buftocopyinto, wifi_uart)));

//	Uart_sendstring(buftocopyinto, pc_uart);

	if (strstr(buftocopyinto, "/PING")) 
	{
		Server_Handle((char*)"...PONG",(char*)"200 OK",Link_ID);
		Uart_flush(wifi_uart);
	}
	else if (strstr(buftocopyinto, "/SendBasic"))
	{
		// Rotina pra Receber o Arquivo e salvar no SD
		// Somente Arquivos Textos
		// Recebe até, inclusive, o EOF (CHR(26))

		// Pega o nome do arquivo
		memset(filename,0,12);
		GetDataFromBuffer((char*)"filename=", (char*)"&", buftocopyinto, filename);

		// Procura o content-length
		vPosIni = strstr(buftocopyinto,"Content-Length:");
		indx = 0;
		slen[0] = 0;
		if (vPosIni)
		{
			while (1)
			{
				if (*vPosIni >= 0x30 && *vPosIni <= 0x39)
				{
					slen[indx++] = *vPosIni;
					slen[indx] = 0;
				}
				
				if (*vPosIni < 0x20)
					break;
				
				vPosIni++;
			}
		}
		postLen = atoi(slen);

		// Le o corpo
		timeout = 999999;
		memset(buftocopyinto, 0, 512);
		while (!(Get_after((char*)"MMSJ800BEGINOFFILE", (postLen - 18), buftocopyinto, wifi_uart)) && timeout) timeout--;

		if (!timeout)
			strcpy(buftocopyinto, "Incorrect Data Submission Structure\r\n");

		postLen -= 18;

		// Salva Arquivo no Disco
		res = f_open(&basicFile, filename, FA_OPEN_ALWAYS | FA_WRITE);
		if (res == FR_OK)
		{
			res = f_write(&basicFile, buftocopyinto, postLen, &lenSave);
			if (res == FR_OK)
			{
				sprintf(data, "Closing File %s, Size %lu, Written %lu...\r\n", filename, postLen, lenSave);
				Uart_sendstring(data, pc_uart);

				Uart_sendstring((char*)"Returning Response...\r\n", pc_uart);

				res = f_close(&basicFile);
				if (res == FR_OK)
				{
					if (lenSave < postLen)
					{
						sprintf(data, "[301]WARNING! Disk is full, bytesToWrite = %lu, bytesWritten = %lu", postLen, lenSave);
						Server_Handle(data,(char*)"200 OK",Link_ID);
					}
					else
						Server_Handle((char*)"[100]File saved successfully",(char*)"200 OK",Link_ID);
				}
				else
				{
					sprintf(data, "[403][%d]Failed to close file", res);
					Server_Handle(data,(char*)"400 Bad Request",Link_ID);
				}
			}
			else
			{
				sprintf(data, "[401][%d]Failed to save file", res);
				Server_Handle(data,(char*)"400 Bad Request",Link_ID);
			}
		}
		else
		{
			sprintf(data, "[402][%d]Failed to open file to save", res);
			Server_Handle(data,(char*)"400 Bad Request",Link_ID);
		}

		Uart_flush(wifi_uart);
	}
	else if (strstr(buftocopyinto, "/LoadFile"))
	{
		// Rotina pra Enviar Arquivo
		// Somente Arquivos Textos
		// Envia até, inclusive, o EOF (CHR(26))

		// Retorna Resposta
		Server_Handle((char*)"File Sent Successfully",(char*)"200 OK",Link_ID);
	}
	else if (strstr(buftocopyinto, "/Exemplo")) // Apenas Exemplo Rec Parametros
	{
		// Apenas exemplo rec parametro
		/*vPosIni = strstr(buftocopyinto, "/Exemplo");
		if (vPosIni != 0)
		{
			vPosIni += 9;	// Comeca a pegar dados depois da posicao (Len + 1)
			ix = 0;
			sSpeed[ix] = 0;
			while(1)
			{
				if (*vPosIni == ' ')
					break;

				sSpeed[ix++] = *vPosIni++;
				sSpeed[ix] = 0;
			}

			vSpeed = atoi(sSpeed);
		}*/

		// Setar valor PWM
		Server_Handle((char*)"/Exemplo",(char*)"200 OK",Link_ID);
	}
	else
		Server_Handle((char*)"Bad Request",(char*)"400 Bad Request",Link_ID);
}

 

 

 

3 REPLIES 3

@MSilv.1 wrote:

f_close takes a long time and returns FS_DISK_ERR.


So what debugging have you done to find where &  why it does that?

It's open-source - so you can step into the f_close() function ...

Thanks for the reply. I appreciate it. Yes, only after looking at the code and trying to identify where the problem is, I opened the post here on the forum. I didn't identify a problematic point. It seems that when it writes to the disk, it loses some reference or can't access the SD even.

The debug you mentioned, this week I upgraded from cubeide 1.13.0 to 1.17.0, and lost the configuration or changed something, and it doesn't work anymore. It doesn't recognize the ST-LINK. I'll see if I can try to configure it again tonight...

At the same time, I'm doing a hardcode debug, putting messages and showing variables inside the program (sending to usart). I want to see if this way I can at least find the exact location of the delay.

So, I did the hard debug and I reached a dead end. I got to the ff.c file in the f_sync function. It is very slow on the following line, returning FR_DISK_ERR:

if (disk_write(fs->drv, fp->buf, fp->sect, 1) != RES_OK) LEAVE_FF(fs, FR_DISK_ERR);

It is passing ds->drv = 0, I didn't look at fp->buf but it is a character buffer, and in fp->sect it is passing 1747.

I don't know what this disk_write does, because the function is below:

DRESULT disk_write (
BYTE pdrv, /* Physical drive numuber to identify the drive */
const BYTE *buff, /* Data to be written */
DWORD sector, /* Sector address in LBA */
UINT count /* Number of sectors to write */
)
{
DRESULT res;

res = disk.drv[pdrv]->disk_write(disk.lun[pdrv], buff, sector, count);
return res; 
}

 

See that it is part of a struct, and in the struct, this:

typedef struct
{
DSTATUS (*disk_initialize) (BYTE); /*!< Initialize Disk Drive */
DSTATUS (*disk_status) (BYTE); /*!< Get Disk Status */
DRESULT (*disk_read) (BYTE, BYTE*, DWORD, UINT); /*!< Read Sector(s) */
#if _USE_WRITE == 1
DRESULT (*disk_write) (BYTE, const BYTE*, DWORD, UINT); /*!< Write Sector(s) when _USE_WRITE = 0 */
#endif /* _USE_WRITE == 1 */
#if _USE_IOCTL == 1
DRESULT (*disk_ioctl) (BYTE, BYTE, void*); /*!< I/O control operation when _USE_IOCTL = 1 */
#endif /* _USE_IOCTL == 1 */

}Diskio_drvTypeDef;

A pointer to some place that I couldn't find in any source, nothing.

Could someone help me see where this is? Because I couldn't get the debugging to work through st-link... I don't know what version 1.17 did.