2025-02-09 05:20 PM - edited 2025-02-09 05:26 PM
I have a board with stm32f407zgt6. I'm using freertos and fatfs. The board has a connection for an SDCARD, I'm using a 4GB SDCARD with fat32.
For reading, F_open, f_read, f_close, everything works. When I use it to write, f_close takes a long time and returns FS_DISK_ERR.
What do you need, files, the .ioc, the sources, no problem, to help me find the problem? I tried to configure it as correctly as possible, but I think I left something behind.
The write process it's in the file ESP8266_HALL.cpp, this file I put in the body of the post, because the forum did not accept the file for a reason that I did not understand, but I will not fight with the forum, I really want help.
Thank you very much.
PS: f_write return the correct amount of bytes written, with what I ordered to be written. the file, after the f_close error, has 0 bytes on the disk. This happens both for already existing files and for new files
/*
* ESP8266_HAL.c
*
* Created on: Apr 14, 2020
* Author: Controllerstech
*/
#include "UartRingbuffer_multi.h"
#include "ESP8266_HAL.h"
#include "stdio.h"
#include "string.h"
#include "stdlib.h"
#include "fatfs.h"
#include "MCUFRIEND_kbv.h"
extern UART_HandleTypeDef huart1;
extern UART_HandleTypeDef huart2;
extern TIM_HandleTypeDef htim11;
extern TIM_HandleTypeDef htim13;
#define wifi_uart &huart1
#define pc_uart &huart2
#define FORWARD 1
#define BACKWARD 2
#define BRAKE 3
#define RELEASE 4
extern MCUFRIEND_kbv tft;
char buffer[20];
char *Basic_inclusion = (char*)"<!DOCTYPE html> <html>\n<head><meta name=\"viewport\"\
content=\"width=device-width, initial-scale=1.0, user-scalable=no\">\n\
<title>MMSJ800</title>\n<style>html { font-family: Helvetica; \
display: inline-block; margin: 0px auto; text-align: center;}\n\
body{margin-top: 50px;} h1 {color: #444444;margin: 50px auto 30px;}\
h3 {color: #444444;margin-bottom: 50px;}\n.p {font-size: 14px;color: #888;margin-bottom: 10px;}\n\
</style>\n</head>\n<body>\n<h1>MMSJ800</h1>\n";
char *Terminate = (char*)"</body></html>";
/*****************************************************************************************************************************************/
//--------------------------------------------------------------------------------
char ESP_Init (char *SSID, char *PASSWD)
{
char data[80];
Ringbuf_init();
char vError = 0;
Uart_sendstring("\r\n\r\nStarting...\r\n", pc_uart);
tft.print(".");
Uart_sendstring("AT+RST\r\n", wifi_uart);
Uart_sendstring("RESETTING.", pc_uart);
for (int i=0; i<5; i++)
{
HAL_Delay(1000);
}
/********* AT **********/
Uart_flush(wifi_uart);
Uart_sendstring("AT\r\n", wifi_uart);
while(1)
{
if (Wait_for((char*)"OK\r\n", wifi_uart))
{
Uart_sendstring("OK\r\n", pc_uart);
break;
}
else if (Wait_for((char*)"Error\r\n", wifi_uart))
{
Uart_sendstring("Error\r\n", pc_uart);
vError = 1;
break;
}
}
if (vError)
{
tft.print("...Error!!!");
Uart_sendstring("\r\nAT---->ERROR\r\n", pc_uart);
return -1;
}
tft.print(".");
Uart_sendstring("\r\nAT---->OK\r\n", pc_uart);
// tft.fillScreen(TFT_BLACK);
// tft.setCursor(0, 16);
/********* AT+CWJAP="SSID","PASSWD" **********/
Uart_flush(wifi_uart);
Uart_sendstring("connecting... to the provided AP\r\n", pc_uart);
sprintf (data, "AT+CWJAP=\"%s\",\"%s\"\r\n", SSID, PASSWD);
Uart_sendstring(data, wifi_uart);
HAL_Delay(3000);
while(1)
{
if (Wait_for((char*)"OK\r\n", wifi_uart))
break;
else if (Wait_for((char*)"Error\r\n", wifi_uart))
{
vError = 1;
break;
}
}
if (vError)
{
Uart_sendstring("Error Connecting\r\n", pc_uart);
return -1;
}
tft.println(".");
sprintf (data, "Connected to \"%s\"", SSID);
tft.print(data);
Uart_sendstring(data,pc_uart);
Uart_sendstring("\r\n",pc_uart);
/********* AT+CWMODE=1 **********/
Uart_flush(wifi_uart);
Uart_sendstring("AT+CWMODE=1\r\n", wifi_uart);
while(1)
{
if (Wait_for((char*)"OK\r\n", wifi_uart))
break;
else if (Wait_for((char*)"Error\r\n", wifi_uart))
{
vError = 1;
break;
}
}
if (vError)
{
Uart_sendstring("CW MODE---->ERROR\r\n", pc_uart);
return -1;
}
tft.print(".");
Uart_sendstring("CW MODE---->OK\r\n", pc_uart);
/********* AT+CIFSR **********/
/* Uart_flush(wifi_uart);
Uart_sendstring("AT+CIFSR\r\n", wifi_uart);
HAL_Delay(3000);
while(1)
{
if (Wait_for((char*)"CIFSR:STAIP,\"", wifi_uart))
break;
else if (Wait_for((char*)"Error\r\n", wifi_uart))
{
vError = 1;
break;
}
}
if (vError)
{
Uart_sendstring("CIFSR---->ERROR\r\n", pc_uart);
return -1;
}
while (!(Copy_upto((char*)"\"",buffer, wifi_uart)));
while(1)
{
if (Wait_for((char*)"OK\r\n", wifi_uart))
break;
else if (Wait_for((char*)"Error\r\n", wifi_uart))
{
vError = 1;
break;
}
}
if (vError)
{
Uart_sendstring("Error Getting IP\r\n", pc_uart);
return -1;
}
int len = strlen (buffer);
buffer[len-1] = '\0';
sprintf (data, "IP ADDR: %s\r\n", buffer);
Uart_sendstring(data, pc_uart);*/
/********* AT+CIPSTA **********/
Uart_flush(wifi_uart);
Uart_sendstring("Setting Static IP...\r\n", pc_uart);
sprintf (data, "AT+CIPSTA=\"192.168.0.67\",\"192.168.0.1\",\"255.255.255.0\"\r\n");
Uart_sendstring(data, wifi_uart);
HAL_Delay(3000);
while(1)
{
if (Wait_for((char*)"OK\r\n", wifi_uart))
break;
else if (Wait_for((char*)"Error\r\n", wifi_uart))
{
vError = 1;
break;
}
}
if (vError)
{
Uart_sendstring("Error Connecting\r\n", pc_uart);
return -1;
}
tft.print(".");
sprintf (data, "Static IP set to 192.168.0.67\r\n");
Uart_sendstring(data,pc_uart);
/********* AT+CIPMUX **********/
Uart_flush(wifi_uart);
Uart_sendstring("AT+CIPMUX=1\r\n", wifi_uart);
while(1)
{
if (Wait_for((char*)"OK\r\n", wifi_uart))
break;
else if (Wait_for((char*)"Error\r\n", wifi_uart))
{
vError = 1;
break;
}
}
if (vError)
{
Uart_sendstring("CIPMUX---->ERROR\r\n", pc_uart);
return -1;
}
tft.print(".");
Uart_sendstring("CIPMUX---->OK\r\n", pc_uart);
/********* AT+CIPSERVER **********/
Uart_flush(wifi_uart);
Uart_sendstring("AT+CIPSERVER=1,80\r\n", wifi_uart);
while(1)
{
if (Wait_for((char*)"OK\r\n", wifi_uart))
break;
else if (Wait_for((char*)"Error\r\n", wifi_uart))
{
vError = 1;
break;
}
}
if (vError)
{
Uart_sendstring("CIPSERVER---->ERROR\r\n", pc_uart);
return -1;
}
tft.println(".");
tft.print(data);
Uart_sendstring("CIPSERVER---->OK\r\n", pc_uart);
Uart_sendstring("Now Connect to the IP ADRESS\r\n", pc_uart);
return 0;
}
//--------------------------------------------------------------------------------
int Server_Send (char *str, int Link_ID)
{
int len = strlen (str);
char data[80];
sprintf (data, "AT+CIPSEND=%d,%d\r\n", Link_ID, len);
Uart_sendstring(data, wifi_uart);
while (!(Wait_for((char*)">", wifi_uart)));
Uart_sendstring (str, wifi_uart);
while (!(Wait_for((char*)"SEND OK", wifi_uart)));
sprintf (data, "AT+CIPCLOSE=5\r\n");
Uart_sendstring(data, wifi_uart);
while (!(Wait_for((char*)"OK\r\n", wifi_uart)));
return 1;
}
//--------------------------------------------------------------------------------
void Server_Handle (char *str, char *resphttpcode, int Link_ID)
{
int len = strlen (str);
char response[200];
sprintf(response,
"HTTP/1.1 %s\r\n"
"Content-Type: text/plain\r\n"
"Content-Length: %d\r\n"
"Connection: close\r\n"
"\r\n"
"%s", resphttpcode, len, str);
Server_Send(response, Link_ID);
}
//--------------------------------------------------------------------------------
void Server_Start (void)
{
char buftocopyinto[512] = {0};
char Link_ID, cRec;
int ix, indx;
unsigned int postLen, lenSave, vhead, vtail, timeout;
char* vPosIni;
char data[320];
char slen[10];
char filename[12];
FIL basicFile;
FRESULT res;
while (!(Get_after((char*)"+IPD,", 1, &Link_ID, wifi_uart)));
Link_ID -= 48;
while (!(Copy_upto((char*)"\r\n\r\n", buftocopyinto, wifi_uart)));
// Uart_sendstring(buftocopyinto, pc_uart);
if (strstr(buftocopyinto, "/PING"))
{
Server_Handle((char*)"...PONG",(char*)"200 OK",Link_ID);
Uart_flush(wifi_uart);
}
else if (strstr(buftocopyinto, "/SendBasic"))
{
// Rotina pra Receber o Arquivo e salvar no SD
// Somente Arquivos Textos
// Recebe até, inclusive, o EOF (CHR(26))
// Pega o nome do arquivo
memset(filename,0,12);
GetDataFromBuffer((char*)"filename=", (char*)"&", buftocopyinto, filename);
// Procura o content-length
vPosIni = strstr(buftocopyinto,"Content-Length:");
indx = 0;
slen[0] = 0;
if (vPosIni)
{
while (1)
{
if (*vPosIni >= 0x30 && *vPosIni <= 0x39)
{
slen[indx++] = *vPosIni;
slen[indx] = 0;
}
if (*vPosIni < 0x20)
break;
vPosIni++;
}
}
postLen = atoi(slen);
// Le o corpo
timeout = 999999;
memset(buftocopyinto, 0, 512);
while (!(Get_after((char*)"MMSJ800BEGINOFFILE", (postLen - 18), buftocopyinto, wifi_uart)) && timeout) timeout--;
if (!timeout)
strcpy(buftocopyinto, "Incorrect Data Submission Structure\r\n");
postLen -= 18;
// Salva Arquivo no Disco
res = f_open(&basicFile, filename, FA_OPEN_ALWAYS | FA_WRITE);
if (res == FR_OK)
{
res = f_write(&basicFile, buftocopyinto, postLen, &lenSave);
if (res == FR_OK)
{
sprintf(data, "Closing File %s, Size %lu, Written %lu...\r\n", filename, postLen, lenSave);
Uart_sendstring(data, pc_uart);
Uart_sendstring((char*)"Returning Response...\r\n", pc_uart);
res = f_close(&basicFile);
if (res == FR_OK)
{
if (lenSave < postLen)
{
sprintf(data, "[301]WARNING! Disk is full, bytesToWrite = %lu, bytesWritten = %lu", postLen, lenSave);
Server_Handle(data,(char*)"200 OK",Link_ID);
}
else
Server_Handle((char*)"[100]File saved successfully",(char*)"200 OK",Link_ID);
}
else
{
sprintf(data, "[403][%d]Failed to close file", res);
Server_Handle(data,(char*)"400 Bad Request",Link_ID);
}
}
else
{
sprintf(data, "[401][%d]Failed to save file", res);
Server_Handle(data,(char*)"400 Bad Request",Link_ID);
}
}
else
{
sprintf(data, "[402][%d]Failed to open file to save", res);
Server_Handle(data,(char*)"400 Bad Request",Link_ID);
}
Uart_flush(wifi_uart);
}
else if (strstr(buftocopyinto, "/LoadFile"))
{
// Rotina pra Enviar Arquivo
// Somente Arquivos Textos
// Envia até, inclusive, o EOF (CHR(26))
// Retorna Resposta
Server_Handle((char*)"File Sent Successfully",(char*)"200 OK",Link_ID);
}
else if (strstr(buftocopyinto, "/Exemplo")) // Apenas Exemplo Rec Parametros
{
// Apenas exemplo rec parametro
/*vPosIni = strstr(buftocopyinto, "/Exemplo");
if (vPosIni != 0)
{
vPosIni += 9; // Comeca a pegar dados depois da posicao (Len + 1)
ix = 0;
sSpeed[ix] = 0;
while(1)
{
if (*vPosIni == ' ')
break;
sSpeed[ix++] = *vPosIni++;
sSpeed[ix] = 0;
}
vSpeed = atoi(sSpeed);
}*/
// Setar valor PWM
Server_Handle((char*)"/Exemplo",(char*)"200 OK",Link_ID);
}
else
Server_Handle((char*)"Bad Request",(char*)"400 Bad Request",Link_ID);
}
2025-02-10 01:56 AM
@MSilv.1 wrote:f_close takes a long time and returns FS_DISK_ERR.
So what debugging have you done to find where & why it does that?
It's open-source - so you can step into the f_close() function ...
2025-02-10 03:26 AM - edited 2025-02-10 05:44 AM
Thanks for the reply. I appreciate it. Yes, only after looking at the code and trying to identify where the problem is, I opened the post here on the forum. I didn't identify a problematic point. It seems that when it writes to the disk, it loses some reference or can't access the SD even.
The debug you mentioned, this week I upgraded from cubeide 1.13.0 to 1.17.0, and lost the configuration or changed something, and it doesn't work anymore. It doesn't recognize the ST-LINK. I'll see if I can try to configure it again tonight...
At the same time, I'm doing a hardcode debug, putting messages and showing variables inside the program (sending to usart). I want to see if this way I can at least find the exact location of the delay.
2025-02-10 01:14 PM
So, I did the hard debug and I reached a dead end. I got to the ff.c file in the f_sync function. It is very slow on the following line, returning FR_DISK_ERR:
if (disk_write(fs->drv, fp->buf, fp->sect, 1) != RES_OK) LEAVE_FF(fs, FR_DISK_ERR);
It is passing ds->drv = 0, I didn't look at fp->buf but it is a character buffer, and in fp->sect it is passing 1747.
I don't know what this disk_write does, because the function is below:
DRESULT disk_write (
BYTE pdrv, /* Physical drive numuber to identify the drive */
const BYTE *buff, /* Data to be written */
DWORD sector, /* Sector address in LBA */
UINT count /* Number of sectors to write */
)
{
DRESULT res;
res = disk.drv[pdrv]->disk_write(disk.lun[pdrv], buff, sector, count);
return res;
}
See that it is part of a struct, and in the struct, this:
typedef struct
{
DSTATUS (*disk_initialize) (BYTE); /*!< Initialize Disk Drive */
DSTATUS (*disk_status) (BYTE); /*!< Get Disk Status */
DRESULT (*disk_read) (BYTE, BYTE*, DWORD, UINT); /*!< Read Sector(s) */
#if _USE_WRITE == 1
DRESULT (*disk_write) (BYTE, const BYTE*, DWORD, UINT); /*!< Write Sector(s) when _USE_WRITE = 0 */
#endif /* _USE_WRITE == 1 */
#if _USE_IOCTL == 1
DRESULT (*disk_ioctl) (BYTE, BYTE, void*); /*!< I/O control operation when _USE_IOCTL = 1 */
#endif /* _USE_IOCTL == 1 */
}Diskio_drvTypeDef;
A pointer to some place that I couldn't find in any source, nothing.
Could someone help me see where this is? Because I couldn't get the debugging to work through st-link... I don't know what version 1.17 did.