Stm324x9I-Eval Ethernet Link Software Interrupt
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-09-23 4:04 AM
Hello,
Kindly guide me in resolving the following issue.
I am working on STM324x9I-Eval board Ethernet example using LwIP example.
On connecting/disconnecting the Ethernet cable from connector CN10 on the board, I wanted an software interrupt to get generated.
Is there any example that serves the purpose.
thanks
Jagdish
#stm32f4 #ethernet- Labels:
-
Ethernet
-
STM32F4 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-09-23 5:04 AM
This is not a straightforward task given the wiring of this board (mine is 429I), follow these steps:
1) Get communication with the IO expander (using i2C bus) 2) Init IO expander to set I/O1(normally connected to the INT output of the PHY) as input and generating an interrupt 3) Install an interrupt handler for IO expander (EXTI8 source on multiplexed EXTI9_5_IRQHandler) 4) Use MDIO channel of EMAC to communicate with the PHY 5) Initialize PHY to generate an interrupt on link status update When you catch the interrupt: 1) Verify on EXTI controller that the source is EXTI8 2) Check on IO expander that it come from I/O1 3) Read PHY status- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-09-23 8:55 PM
Is there any link available that shares such implementation of initializing and usage of IO expander.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-09-24 12:05 AM
The minimum steps required to initialize the IOEXP (given that we have the same STMPE1600) is to enable interrupt on the IO/1 and enable generation of external interrupts:
IOEXP_write8(IEGPIOR_LSB,1<<1); IOEXP_write8(SYSTEM_CONTROL, 4); The write function is a generic I2C write function using the Standard Peripheral Lib:void IOEXP_write8(uint8_t regnum, uint8_t value)
{
I2C_GenerateSTART(I2C1, ENABLE);
while ( I2C_GetFlagStatus(I2C1, I2C_FLAG_SB) == RESET );
I2C_Send7bitAddress(I2C1, IOEXP_ADDR*2, I2C_Direction_Transmitter);
while ( I2C_GetFlagStatus(I2C1, I2C_FLAG_ADDR) == RESET );
I2C_GetFlagStatus(I2C1, I2C_FLAG_MSL);
while ( I2C_GetFlagStatus(I2C1, I2C_FLAG_TXE) == RESET );
I2C_SendData(I2C1, regnum);
while ( I2C_GetFlagStatus(I2C1, I2C_FLAG_TXE) == RESET );
I2C_SendData(I2C1, value);
while ( I2C_GetFlagStatus(I2C1, I2C_FLAG_TXE) == RESET );
I2C_GenerateSTOP(I2C1, ENABLE);
while ( I2C_GetFlagStatus(I2C1, I2C_FLAG_BUSY) == SET );
}