2018-04-24 5:56 AM
Hello guys,
I am using de STM32DiscoveryF4 in my project and the CC2564MODN bluetooth module with the adapter kit to make a bluetooth serial port profile with the API's that TI brings (SPPLE), but once the code is flashed and the board programmed I can't make the COM port appear, even connecting the micro-usb to the PC too.
I read the API documentacion, 'Enable_STM32_Discovery.pdf' and make all the changes that I've to.
- Device, HSE_VALUE
- HALCFG.h
- Put the Bluetopia/hcitrans/HCITRANS.c
- HCITRCFG.h
I install the driver that ST brings which is STSW-009, to program via miniUSB, but it only flashed the code into the board it doesn't open any COM port when I plugged the miniUSB again or the micro-usb to the PC and reset the board.
In the API's demo example says that 'Once the code is flashed, connect the board to a PC using a miniUSB or microUSB cable. Once connected, wait for the driver to install. It will show up as MSP-EXP430F5438 USB - Serial Port(COM x), Tiva Virtual COM Port (COM x), XDS110 Class Application/User UART (COM x) for MSP432, under Ports (COM & LPT) in the Device manager.'
So reading that I tough that just flashing the code into the board It will make the COM port appear, when a I plugged the microUSB but don't happen.
So, I ask if someone has the same problem and know how to resolve it, please contact to me and let me know. ASAP !!
Regards and thanks.
#stm32f4-bluetooth #stm-32 #stm32f4 #vcp-driver-stm32 #bluetooth-low-energy #stm32f4-discovery2018-04-24 6:04 AM
I'm programming with the Keil uvision 4 and using the API: 'CC256x STM32 Bluetopia SDK v4.0.2.2'