2016-05-22 1:50 AM
Hi all,
i am using a Nucleo board ''NUCLEO F070RB'' and i want to start the UART Bootloader. Unfortunately the bootloader doesn�t send the Ack byte (0x79) after activation.My procedure to start the bootloader:- connect the boot0 pin to 3V3- reset the board (black botton)- send the 0x7F Byte with 9600, even parity, 1 start bit, 1 stop bit=> at this point i expect to receive the 0x79 ACK byte from the microWhat i did till now to find what i am doing wrong:- i checked that nBOOT1 bit in the option bytes is set to 1- due to the fact that the F070 device has an USB interface i removed the crystal (and i opened SB50 from the NUCLEO to avoid getting clock from the debugger)- i am quite sure that the micro is in bootloader mode, because the application doesn�t start.- i verified my sequence with a NUCLEO-F030RB=> here erverything works fine. The problem just excists on the F070.=> all my HW-connections should be ok (same Pins)I am running out of ideas :( Any help is appreciated.ThanksThomas #nucleo-f070rb #bootloader2016-05-23 5:51 AM
Which Pins and USART are being utilized?
Can you identify the ROM version being used? What are the marking/production codes from the top of the device?2016-05-23 6:40 AM
Hi jung.thomas.001
In , section'' STM32F070xB devices bootloaders'' p 44, there is a note: '' Note: If HSI deviation exceeds 1% , the bootloader might not function correctly. '' So It may the HSI of the device is not accurate enough, try with a HSE crystal. -Hannibal-2016-05-23 11:24 PM
Hi clive1,
thanks for the replay.I am using USART1 on PA9 and PA10. I use the same USART and the same pins in my application and there it works fine. Same connections on a NUCLEO F030 board works fine.How can i identify the ROM Code Version? Is it part of the production code? This evening i will send you the production code. I don´t have the board with me. I tried at least two boards.ThanksThomas2016-05-23 11:33 PM
Hi Hannibal,
thanks for the replay.i have read the note you mentioned, therefore i tried both, with and without crystal. Nothing works. Is there any other possibility to skip the USB bootloader. What is the indication for the bootloader to detect a connected USB interface (PA11, PA12, PA13) ?ThanksThomas2016-05-24 8:24 AM
Hi clive1,
here is the product code: STM32F070R8T6 GH262 98 CHN GH 447 The code is the same for all the boards i have tried. Thanks for help Thomas2016-05-24 9:34 AM
The USART1 should be functional with HSI, one might try different baud rates. Connecting it via a VCP might be problematic, the bootloader will be sensitive to glitches as the 0x7F is a pattern that is being measured, rather than received. You could use a scope to see if there is an 0x79 response at some other baud rate.
Absent USART/USB connectivity to the loader to query its version, one would have to download via SWD and manually dig it out. The ROM is 12KB located at 0x1FFFC800..0x1FFFF7FF[0x3000]Not a part I'm using, but the codes should let someone at ST identify if there is a parts/batch issue.2016-05-24 10:29 AM
Hi clive1,
the USART is connected to a FTDI Evalboard ''UM232R'' which is mounted nearby the NUCLEO board. I already checked the RX and TX line with my scope. I see a perfect 0x7F on the RX line bt nothing (constant high) on the TX line. I also checked different baud rates (9600, 115200). I checked the bootloader Version. (Adress 0x1ffff6a6 Version: 0xA2). This is what i expect. AN2606 tells me that it should be USART bootloader Version 3.1. Do you Need more numbers from the bootloadercode? We could also debug the bootloader. I could set breakpoints and see if we hit them. Thanks for help Thomas2016-05-30 3:41 AM
Hi all,
somebody else who has an idea??ThanksThomas2017-06-13 2:43 AM
Hi Thomas
Do you find the problem ? I am the same problem, the boot0 is hight but the stm32f070cb doesnt respond in bootmode.
Thanks.
Julien