Problem with Ethernet connection (STM32F417 + LwIP + LAN8720)
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2017-08-28 9:06 AM
Posted on August 28, 2017 at 18:06
Hello,
I am building a system with ethernet on a STM32F417. When I connect the circuit to my PC directly, the connection is established successfully when my ethernet cable has no ground connected to the shield. When I connect it with a cable where the shield is connected, the connection can not be established, both Ethernet LEDs are constantly on.
When I connect it to a switch, there is a similar problem. Independent of the cable, the LEDs are constantly on and no connection to the network is possible.
Has anybody an idea?
Best regards
#switch #stm32f4 #ethernet #lwip
Labels:
- Labels:
-
Ethernet
-
STM32F4 Series
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0