2014-07-29 9:16 AM
I am a beginner with Stm32f4discovery (version stm32f407vg). It took me a long to get the graphic LCD work (copying and rewriting some code from others).
My problem, I want to use it with FreeRTOS. But My FreeRTOS works in Stm32Cube. And my GLCD works in stm32f4firmware. I tried a lot but I can not get FreeRTOS in Stm32f4 firmware in IAR/arm, nor can I get GLCD work with Stm32cube in Keil.My question. Who can help to rewrite the following code in stm32cubef4? Please help me. Alternatively, who can send me a working project with freertos, stm32f4 firmware in iar/arm. Here is the code:static void LCD_CtrlLinesConfig(void){ GPIO_InitTypeDef GPIO_InitStructure; /* Enable GPIOs clock */ RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOD | RCC_AHB1Periph_GPIOE , ENABLE); /* Enable FSMC clock */ RCC_AHB3PeriphClockCmd(RCC_AHB3Periph_FSMC, ENABLE); /*-- GPIOs Configuration ------------------------------------------------------*/ /* +-------------------+--------------------+------------------+------------------+ + SRAM pins assignment + +-------------------+--------------------+ */ /* GPIOD configuration */ /* Set PD.00(D2), PD.01(D3), PD.04(NOE), PD.05(NWE), PD.08(D13), PD.09(D14), PD.10(D15), PD.11(A16), PD.14(D0), PD.15(D1) as alternate function push pull */ GPIO_PinAFConfig(GPIOD, GPIO_PinSource0, GPIO_AF_FSMC); GPIO_PinAFConfig(GPIOD, GPIO_PinSource1, GPIO_AF_FSMC); GPIO_PinAFConfig(GPIOD, GPIO_PinSource4, GPIO_AF_FSMC); GPIO_PinAFConfig(GPIOD, GPIO_PinSource5, GPIO_AF_FSMC); GPIO_PinAFConfig(GPIOD, GPIO_PinSource8, GPIO_AF_FSMC); GPIO_PinAFConfig(GPIOD, GPIO_PinSource9, GPIO_AF_FSMC); GPIO_PinAFConfig(GPIOD, GPIO_PinSource10, GPIO_AF_FSMC); GPIO_PinAFConfig(GPIOD, GPIO_PinSource11, GPIO_AF_FSMC); GPIO_PinAFConfig(GPIOD, GPIO_PinSource14, GPIO_AF_FSMC); GPIO_PinAFConfig(GPIOD, GPIO_PinSource15, GPIO_AF_FSMC); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1 | GPIO_Pin_4 | GPIO_Pin_5 | GPIO_Pin_8 | GPIO_Pin_9 | GPIO_Pin_10 | GPIO_Pin_11 | GPIO_Pin_14 | GPIO_Pin_15; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP; GPIO_Init(GPIOD, &GPIO_InitStructure); /* Set PE.07(D4), PE.08(D5), PE.09(D6), PE.10(D7), PE.11(D8), PE.12(D9), PE.13(D10), PE.14(D11), PE.15(D12) as alternate function push pull */ /* GPIOE configuration */ GPIO_PinAFConfig(GPIOE, GPIO_PinSource2 , GPIO_AF_FSMC); GPIO_PinAFConfig(GPIOE, GPIO_PinSource7 , GPIO_AF_FSMC); GPIO_PinAFConfig(GPIOE, GPIO_PinSource8 , GPIO_AF_FSMC); GPIO_PinAFConfig(GPIOE, GPIO_PinSource9 , GPIO_AF_FSMC); GPIO_PinAFConfig(GPIOE, GPIO_PinSource10 , GPIO_AF_FSMC); GPIO_PinAFConfig(GPIOE, GPIO_PinSource11 , GPIO_AF_FSMC); GPIO_PinAFConfig(GPIOE, GPIO_PinSource12 , GPIO_AF_FSMC); GPIO_PinAFConfig(GPIOE, GPIO_PinSource13 , GPIO_AF_FSMC); GPIO_PinAFConfig(GPIOE, GPIO_PinSource14 , GPIO_AF_FSMC); GPIO_PinAFConfig(GPIOE, GPIO_PinSource15 , GPIO_AF_FSMC); GPIO_InitStructure.GPIO_Pin =GPIO_Pin_2 | GPIO_Pin_7 | GPIO_Pin_8 | GPIO_Pin_9 | GPIO_Pin_10 | GPIO_Pin_11| GPIO_Pin_12 | GPIO_Pin_13 | GPIO_Pin_14 | GPIO_Pin_15; GPIO_Init(GPIOE, &GPIO_InitStructure); /*The following code is not necessary since PD7 is FSMC_NE1 */ /* GPIO_InitStructure.GPIO_Pin = GPIO_Pin_7; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_100MHz; GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP; GPIO_Init(GPIOD, &GPIO_InitStructure); GPIO_ResetBits(GPIOD,GPIO_Pin_7); */}/******************************************************************************** Function Name : LCD_FSMCConfig* Description : Configures the Parallel interface (FSMC) for LCD(Parallel mode)* Input : None* Output : None* Return : None* Attention : None*******************************************************************************/static void LCD_FSMCConfig(void){ FSMC_NORSRAMInitTypeDef FSMC_NORSRAMInitStructure; FSMC_NORSRAMTimingInitTypeDef FSMC_NORSRAMTimingInitStructure; FSMC_NORSRAMInitStructure.FSMC_Bank = FSMC_Bank1_NORSRAM4; FSMC_NORSRAMInitStructure.FSMC_DataAddressMux = FSMC_DataAddressMux_Disable; FSMC_NORSRAMInitStructure.FSMC_MemoryType = FSMC_MemoryType_SRAM; FSMC_NORSRAMInitStructure.FSMC_MemoryDataWidth = FSMC_MemoryDataWidth_16b; FSMC_NORSRAMInitStructure.FSMC_BurstAccessMode = FSMC_BurstAccessMode_Disable; FSMC_NORSRAMInitStructure.FSMC_WaitSignalPolarity = FSMC_WaitSignalPolarity_Low; FSMC_NORSRAMInitStructure.FSMC_WrapMode = FSMC_WrapMode_Disable; FSMC_NORSRAMInitStructure.FSMC_WaitSignalActive = FSMC_WaitSignalActive_BeforeWaitState; FSMC_NORSRAMInitStructure.FSMC_WriteOperation = FSMC_WriteOperation_Enable; FSMC_NORSRAMInitStructure.FSMC_WaitSignal = FSMC_WaitSignal_Disable; FSMC_NORSRAMInitStructure.FSMC_AsynchronousWait = FSMC_AsynchronousWait_Disable; FSMC_NORSRAMInitStructure.FSMC_ExtendedMode = FSMC_ExtendedMode_Disable; FSMC_NORSRAMInitStructure.FSMC_WriteBurst = FSMC_WriteBurst_Disable; FSMC_NORSRAMInitStructure.FSMC_ReadWriteTimingStruct = &FSMC_NORSRAMTimingInitStructure;// FSMC_NORSRAMInit(&FSMC_NORSRAMInitStructure); /* FSMCд�ٶ����� */ FSMC_NORSRAMTimingInitStructure.FSMC_AddressSetupTime = 15;//1; /* ��ַ����ʱ�� */ FSMC_NORSRAMTimingInitStructure.FSMC_AddressHoldTime = 0; FSMC_NORSRAMTimingInitStructure.FSMC_DataSetupTime = 15;//1; /* ���ݽ���ʱ�� */ FSMC_NORSRAMTimingInitStructure.FSMC_BusTurnAroundDuration = 0x00; FSMC_NORSRAMTimingInitStructure.FSMC_CLKDivision = 0x00; FSMC_NORSRAMTimingInitStructure.FSMC_DataLatency = 0x00; FSMC_NORSRAMTimingInitStructure.FSMC_AccessMode = FSMC_AccessMode_A; /* FSMC ����ģʽ */ FSMC_NORSRAMInitStructure.FSMC_WriteTimingStruct = &FSMC_NORSRAMTimingInitStructure; FSMC_NORSRAMInit(&FSMC_NORSRAMInitStructure); /* Enable FSMC Bank4_SRAM Bank */ FSMC_NORSRAMCmd(FSMC_Bank1_NORSRAM4, ENABLE); } #stm32f4discovery #cube2014-07-29 9:42 AM
My question. Who can help to rewrite the following code in stm32cubef4? Please help me. Alternatively, who can send me a working project with freertos, stm32f4 firmware in iar/arm.
I have about zero interest in free cube support, but did port FreeRTOS 7.1.1 to the F2/F4 and the F4-DISCO in Keil using the standard firmware. You might want to look over the F4 Ethernet IAP example, it includes FreeRTOS 7.3.0 [DEAD LINK /public/STe2ecommunities/mcu/Lists/STM32F4DISCOVERY/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/STM32F4DISCOVERY/Demo%20FreeRTOS%20on%20STM32F4%20Discovery&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580002E3D0FFCC5A9AA4A9C29C3EECB7CCDBF¤tviews=8366]https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32F4DISCOVERY/Flat.aspx?RootFolder=%2Fpublic%2FSTe2ecommunities%2Fmcu%2FLists%2FSTM32F4DISCOVERY%2FDemo%20FreeRTOS%20on%20STM32F4%20Discovery&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580002E3D0FFCC5A9AA4A9C29C3EECB7CCDBF¤tviews=83662014-07-29 9:51 AM
Sorry for raising this type of request. But thanks a lot for the hint. I will sure study the examples as you pointed out.
2014-07-29 11:20 AM
I used the Ethernet Example, delected everything but just left the freertos to switch an led.
It worked. But I do have an issure here. Problem: xSemaphoreHandle,no where can i find out where it is defined in the project folder.2014-07-29 12:22 PM
STM32F4x7_ETH_LwIP_V1.1.0\Utilities\Third_Party\FreeRTOSV7.3.0\include\semphr.h