2025-09-29 6:33 PM
Hello,
I have a project using the spirit MP3 Decoder. I am in the process of moving this project over to a FreeRTOS based project using the STM32F411. FreeRTOS only supports hardware floating point for this chip and the spirit MP3 decoder is provided as a library only supporting software floating point.
What is required for me to get a new build of the Spirit MP3 deocder re-compiled supporting hardware floating point?
Can ST provide this re-compiled library?
Thanks
Stuart
2025-09-30 4:00 AM
Almost the same question was asked here.
2025-09-30 5:05 PM
Yeah, i saw the post, but in the response it says that the company doesn't exist anymore....
But they do have a website.
Can you confirm that this is the same company? (their logo is the same)
Thanks
2025-11-28 7:34 AM
@SORei.1 wrote:
Can you confirm that this is the same company? (their logo is the same)
Most probably yes. To my knowledge the company name is DSP spirit.