2015-10-09 6:39 AM
Hi all,
I am newbie in stm32f411e-disco and sw4stm32.I am trying to write a audio playback program in my board, but I met some problem in using BSP_Audio_In_Init() and BSP_Audio_Out_Init().This is how I start my program:1. Create new C program with project's name ''audioTest'', and choose ''Ac6 STM32 MCU GCC'' as Toolchain.2.In MCU Configuration, ''STM32F411E-Disco'' was chosen directly.3. In Project Firmware Configuration, ''CubeHAL'' was chosen and ''STM32_Audio'' as additional driver.The rest remain unchanged.In project properties,1. I updated the Linker Script to ''STM32F411VETx_FLASH.ld'', which I get from CubeMX2. I added '':libPDMFilter_CM4F_GCC.a'' to librariesThe rest remain unchangedWhat I want it to do in my program is:1. toggle 4 LEDs (LED3,4,5,6) until Pushbutton is press2. Call Audio_In_Init() (or Audio_Out_Init()).3. IF call FAIL, Led3 will on. (false case) ELSE both Led3 and Led4 will on. (true case)here is my main.c:int main(void)
{ HAL_Init(); SystemClock_Config(); BSP_LED_Init(LED3); BSP_LED_Init(LED4); BSP_LED_Init(LED5); BSP_LED_Init(LED6); BSP_PB_Init(BUTTON_KEY,BUTTON_MODE_EXTI); while (!UserPressButton)Toggle_Leds(); if(BSP_AUDIO_IN_Init(DEFAULT_AUDIO_IN_FREQ, DEFAULT_AUDIO_IN_BIT_RESOLUTION, DEFAULT_AUDIO_IN_CHANNEL_NBR) != AUDIO_OK){ //if (BSP_AUDIO_OUT_Init(OUTPUT_DEVICE_AUTO, DEFAULT_VOLMAX, AUDIO_FREQUENCY_16K)!= 0) BSP_LED_On(LED3); } else{ BSP_LED_On(LED3); BSP_LED_On(LED4); } for(;;); } My code was compiled and built successfully, and when I port it to my stm32f411e-disco, leds was toggling as my expectation.However, when I press the pushbutton, the LED stop toggling, but neither true case nor false case present. The LEDs just remain their state when I press the pushbutton.I know program stop at calling BSP_Audio_In/Out_Init() function, but I don't know why this happen and how to fix it.Can anyone help me and give me some advices?Here I uploaded my full set of 'audioTest'project:https://www.dropbox.com/sh/7fx7cu3ko5wtrn8/AACmi_OFUGxJYTuIJohumWWXa?dl=0Thank you very much #audio #sw4stm32 #stm32f411e-disco2015-10-28 6:37 AM
Hi sim.kae_wanq,
It will be more interesting if you let us know how you resolved the case. It may be helpful for other forum users; and this is one of forum's purposes.-Syrine-