cancel
Showing results for 
Search instead for 
Did you mean: 

Reading adc channels for temp e vref gives same value

SGasp.1
Senior

Hi amazing comminity.. 

I have configured the adc for reading the internal temp and vref in the following way ..

 

 

 

 

void MX_ADC_temp_Init(void)
{
	  /* USER CODE BEGIN ADC1_Init 0 */

	  /* USER CODE END ADC1_Init 0 */

	  ADC_ChannelConfTypeDef sConfig = {0};

	  /* USER CODE BEGIN ADC1_Init 1 */

	  /* USER CODE END ADC1_Init 1 */

	  /** Configure the global features of the ADC (Clock, Resolution, Data Alignment and number of conversion)
	  */
	  hadc1.Instance = ADC1;
	  hadc1.Init.ScanConvMode = ADC_SCAN_DISABLE;
	  hadc1.Init.ContinuousConvMode = ENABLE;
	  hadc1.Init.DiscontinuousConvMode = DISABLE;
	  hadc1.Init.ExternalTrigConv = ADC_SOFTWARE_START;
	  hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT;
	  hadc1.Init.NbrOfConversion = 1;

	  if (HAL_ADC_Init(&hadc1) != HAL_OK)
	  {
	    Error_Handler();
	  }

	  // Configure ADC channel for temperature sensor
	  sConfig.Channel = ADC_CHANNEL_TEMPSENSOR;
	  sConfig.Rank = ADC_REGULAR_RANK_1;
	  sConfig.SamplingTime = ADC_SAMPLETIME_239CYCLES_5;

	  if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
	  {
	    Error_Handler();
	  }

	  // Configure ADC channel for internal voltage reference (VREF)
	  sConfig.Channel = ADC_CHANNEL_VREFINT;
	  sConfig.Rank = ADC_REGULAR_RANK_2;
	  sConfig.SamplingTime = ADC_SAMPLETIME_239CYCLES_5;

	  if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
	  {
	    Error_Handler();
	  }

}

 

 

 

 Then i execute the following code for reading the 2 channels.. 

 

 

 

 

MX_ADC_temp_Init();

		/*start of adc*/
		HAL_ADC_Start(&hadc1);
		HAL_ADC_PollForConversion(&hadc1, HAL_MAX_DELAY);
		raw_temp_value_mcu = HAL_ADC_GetValue(&hadc1);
		HAL_ADC_PollForConversion(&hadc1, HAL_MAX_DELAY);
		raw_vref_mcu = HAL_ADC_GetValue(&hadc1);
		/*final computation of mcu temp*/
		mcu_temperature = mcu_get_temperature(raw_temp_value_mcu, raw_vref_mcu);

 

 

 

 It seems when i look to the raw adc values that is always the ssame value (raw_temp_value_mcu) and raw_vref_mcu are very similar as it is always reading the same channel . 

 

What could be wrong here ? 

 

Thanks a lot for your support @Tesla DeLorean 

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Amel NASRI
ST Employee

Hi @SGasp.1 ,

Calling HAL_ADC_PollForConversion will clear ADC flag EOS (ADC group regular end of sequence conversion).
So it needs to be called only one time after the last HAL_ADC_GetValue.

You can also use the DMA with ADC. A ready to use example is available in https://github.com/STMicroelectronics/STM32CubeL4/tree/master/Projects/NUCLEO-L496ZG/Examples/ADC/ADC_Sequencer. In this example, 3 channels are converted: one external channel and two internal channels (VrefInt and temperature sensors).

You didn't mention the used hardware, but you may find a similar example for your device in the relevant STM32Cube package.

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.