cancel
Showing results for 
Search instead for 
Did you mean: 

Programming demo application via DfuSe

mariemzidi
Associate II
Posted on April 13, 2010 at 16:26

Programming demo application via DfuSe

#dfuse-v3.0.0
11 REPLIES 11
Posted on May 17, 2011 at 13:46

Rather than continually spamming the forum with the same question, perhaps you should contact your local ST-Micro FAE for support?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
yagov
Associate II
Posted on May 17, 2011 at 13:46

I had the same problems.

Before the following instruction load this project to your board.

C:\Program Files\Raisonance\Ride\Examples\ARM\STM3210B-EVAL\STM32F10xUSBLib\USBLib\demos\Device_Firmware_Upgrade\project\RIDE (if your Ride is in the other place or you have no ride and use another tool - find the same folder)

There is a project, that you muct download to the controller before using DEFUSE.

run it and follow the instruction.
mariemzidi
Associate II
Posted on May 17, 2011 at 13:46

I do contact my local st support but withoutany reply !!!

mariemzidi
Associate II
Posted on May 17, 2011 at 13:46

Hi Denis,

Thanx for your help !!

Hope it will woks..

Best Regards

mariemzidi
Associate II
Posted on May 17, 2011 at 13:46

Hi Denis,

I already Loaded the Device_Firmware_Project to the board but when I run the DfuSe (3.0 Version)

I found some fields missing like the ''select target field'' and the ''Available Dfu field ''

There is the interface attached; I think probably I have a problem with the DfuSe

Looking forward to hearing from you

yagov
Associate II
Posted on May 17, 2011 at 13:46

Hello.

I dont think that the problem in the DFU program.

SD - card is in the board?

can you leave the DFU mode?
yagov
Associate II
Posted on May 17, 2011 at 13:46

Zidi. I know your problem.

You didn`t enterd to Defuse mode before run the DEFUSE program.

You must press the ''user button'' and click the ''reset button'' after that push out the ''user button''

In this case the program in the target enters to DEFUSE mode.

(As I remember, this procedure has been written in the manual)

Then run the DEFUSE program on PC.

You ll see that no window components absent.

MAKE IT!

As I remember, there is another one problem in the final of instalation. But I ll tell you about it when (and if) you ll get it.

mariemzidi
Associate II
Posted on May 17, 2011 at 13:47

Hi Denis,

Thank you very much! I really appreciate your help !!

I make it with the demo and it is working proporly, the problem was in the DFU program I made some changes according to the target and everything is OK :)

mariemzidi
Associate II
Posted on May 17, 2011 at 13:47

By the way, I want to ask you did you work also with DFU Files?

because I need to make some changes in the file according to my application,

Do you Know which software I should use to open and manage those files (.dfu) ?

Best Regards

Mariem