Problem with UART HAL DRIVER function.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2015-05-24 3:35 PM
Hi, i was trying to learn how to use the UART from m stm32f429DISCO, starting with a simple polling program that reads a caracter from pc and retransmit it. (i've reviewed reference manual, datasheet and the description of hal drivers pdf) but can't find the reason why the HAL_UART_Receive(); doesnt change the rxbuffer at all.
I use abother board as usb to 232 converter and coolterm to send the data.I've used cubeMX to configure UART 7 port and verified how it set my GPIOF pins 6 and 7 as RX and TX. I've checked the uart configuration matching in my coolterm and the program. and used the solution suggested byHeisenberg in
/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Best%20way%20to%20use%20HAL%20UART%20Receiver%20IT%20Function&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B¤tviews=4963
/* Includes ------------------------------------------------------------------*/&sharpinclude ''stm32f4xx_hal.h''/* USER CODE BEGIN Includes *//* Private variables ---------------------------------------------------------*/UART_HandleTypeDef huart7;void SystemClock_Config(void);static void MX_GPIO_Init(void);static void MX_UART7_Init(void);int main(void){ /* Reset of all peripherals, Initializes the Flash interface and the Systick. */ HAL_Init(); /* Configure the system clock */ SystemClock_Config(); /* Initialize all configured peripherals */ MX_GPIO_Init(); MX_UART7_Init(); /* USER CODE BEGIN 2 */ /* USER CODE END 2 */ /* Infinite loop */ /* USER CODE BEGIN WHILE */ uint8_t aTxBuffer[2]; aTxBuffer[0]=0x30; aTxBuffer[1]=0x31; uint8_t aRxBuffer[2]; HAL_StatusTypeDef UARTStatus; while (1){ UARTStatus = HAL_UART_Receive(&huart7,(uint8_t *)aRxBuffer, 2, 5000); while((UARTStatus != HAL_OK) || (UARTStatus != HAL_TIMEOUT)){ aTxBuffer[0]=aTxBuffer[0]+aRxBuffer[0]; aTxBuffer[1]=aTxBuffer[1]+aRxBuffer[1]; UARTStatus2=HAL_UART_Transmit(&huart7,(uint8_t*)aTxBuffer,2, 5000); while((UARTStatus2 != HAL_OK) || (UARTStatus != HAL_TIMEOUT)){ } HAL_UART_Receive(&huart7,(uint8_t *)aRxBuffer, 2, 5000); } }//fwhile }//FMAIN----------------The program is supposed to change what is shown on the terminal in some way but i keep getting the eternal 0101010101and it doesnt change no matter how many keys i press... any ideas of what im doing wrong? #hal #uart #stm32f429 #polling- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2015-05-26 7:54 AM
Hi,
You may be using the HAL functions incorrectly. For example, UARTStatus2=HAL_UART_Transmit(&huart7,(uint8_t*)aTxBuffer,2, 5000); while((UARTStatus2 != HAL_OK) || (UARTStatus != HAL_TIMEOUT)){ }This transmits 2 bytes from the buffer and HAL_UART_Transmit() returns when it's done. So the while() loop is useless (UARTStatus2 will not change after the Transmit call). Maybe you were looking for non-blocking functions ?Also, your first ''while (UARTStatus != OK || UARTStatus != Timeout) {...} '') is suspicious, for the same reason: HAL_UART_Receive() is blocking.- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2015-05-28 8:57 PM
Thanks, got it working now, i had bad understanding of it, now after a few days of reading i'm not doing those silly things anymore. Now im into non blocking mode. Thanks for your interest.