Question
Problem Sending MQTT messages using FreeRTOS
Hello,
I have an FreeRTOS task that sends 4 MQTT messages (using LwIP MQTT) every 10 seconds:
void HomeAssistantConfigTask(void *argument)
{
/* USER CODE BEGIN HomeAssistantConfigTask */
/* Infinite loop */
for(;;)
{
SendAvailabilityMessage();
SendPowerConfigMessage();
SendDisplayConfigMessage();
SendFrontLedConfigMessage();
osDelay(10000);
}
osThreadTerminate(NULL);
/* USER CODE END HomeAssistantConfigTask */
}But most of the times the last 2 messages are not sent... Seems like the thread is being interrupted before sending the message. I also tried to add osDelay between sending messages and I have same problem.
I have in total 4 FreeRTOS tasks and this one is configured like this:
osThreadId_t HMConfigTaskHandle;
const osThreadAttr_t HMConfigTask_attributes = {
.name = "HMConfigTask",
.stack_size = 4096 * 4,
.priority = (osPriority_t) osPriorityAboveNormal2,
};The other tasks are running every 100ms and every 5s.
I'm using STM32F407VGT with FreeRTOS using CMSIS_V2.
Thanks for reading.