2019-09-30 11:26 PM
Hello ,
I have to implement USB mass storage device im my current project
I have done some configuration and generate code
but it seem have some problem
1)usb mass storage device is showon in device manager
2)In my computer also show that drive is connected
but problem is that inspite of opening drive it always asks to format drive
i have attached screenshots of errors with this post.
Thanks
Dipak Garasiya
Solved! Go to Solution.
2019-10-03 4:50 AM
2019-10-03 4:49 AM
i have sort out this problem
Best Regards
Dipak Garasiya
2019-10-03 4:50 AM
if someone has problem , i will guide you
dipak garasiya
2019-10-10 1:31 AM
follow and port accoring to your contoller
C:\Users\Graffin01\STM32Cube\Repository\STM32Cube_FW_F7_V1.15.0\Projects\STM32F769I-Discovery\Applications\USB_Device\MSC_Standalone
2021-06-03 10:35 PM
hi,
I have configured the same interface and it is working.
But I want to show the sd card as write protected. I don't want the files to be edited or deleted when connected to pc.
Can you please suggest a solution for this.
2024-04-18 11:44 AM