Possible problem with ethernetif.c
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2017-04-26 11:24 AM
Posted on April 26, 2017 at 20:24
In the file ethernetif.c supplied as part of cubemx based BSP, there is a static function low_level_output(). In this function is a call to HAL_ETH_TransmitFrame().
The return code of HAL_ETH_TransmitFrame() is not checked. It returns one of the three codes, 0=OK, 1=Error, and 2=HAL_BUSY. The HAL_BUSY code is return via the macro __HAL_LOCK
If HAL_BUSY is returned, there is no 'retry' and no way to report the 'failure'.
This can cause a disruption in TCP/IP communication, should __HAL_LOCK return busy.
#bsp #tcp/ip-stack #cubemx
Labels:
- Labels:
-
Ethernet
0 REPLIES 0