cancel
Showing results for 
Search instead for 
Did you mean: 

PMOD (or Arduino) Ethernet on STM32H747i-disco Board

BillG
Associate II

Has anyone tried to get ethernet over PMOD or perhaps with Arduino working on the STM32747i discovery board? I need ethernet but modifying the solder bridges is not something I can do.

Maybe I could use the STMod+ expansion board and try the mikroBus connector?

Thanks.

-bill

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
S.Ma
Principal

The remote ethernet are spi based, so probably low speed. The 10/100 ethernet of STM32 uses 10 wires and 25Mhz clock. If it is not a production project, the spi click will lower the complexity and development time.