cancel
Showing results for 
Search instead for 
Did you mean: 

osMessagePut problems

Stepan Podhorsky
Associate II
Posted on March 23, 2017 at 12:13

Hello,

I have been trying to solve problem with the osMessagePut function from

CMSIS-RTOS wrapper. I am not able to insert instances of C structure into

the message queue.  

My code is following:

// transmission queue

static

osMessageQId

tx_CAN_Message_queue;

// mutex related to transmission queue  

static

osMutexId

tx_mutex;

// function initializes the task's internal objects

void

Init_Task(

void

){

   // transmission queue

   osMessageQDef(tx_CAN_Message_queue, CAN_BUFFER_LENGTH,

msg_t

);

   tx_CAN_Message_queue = osMessageCreate(osMessageQ(tx_CAN_Message_queue),

NULL

);

   // mutex related to transmission queue  

   osMutexDef(tx_mut);

   tx_mutex = osMutexCreate(osMutex(tx_mut));

}

void

send_single_gdt_read_resp(

uint8_t

blk_index,

uint8_t

rec_index){

   

// created message

   

thb_msg_t

tx_msg;

   

// created packets for the transmitted message

   

thb_pkt_t

tx_pkt_array[MAX_NO_PACKETS];

   uint8_t

i;

   uint8_t

no_packets;

    

can_message_t

can_msg;

   

// prepare the message

   build_single_gdt_msg(

SHORT_SINGLE_GDT_READ_RESP_MSG

, blk_index, rec_index, &tx_msg);

   

// divide the message into packets

   no_packets = calc_no_packets(&tx_msg);

   tx_msg_to_packets(&tx_msg, no_packets, tx_pkt_array);

   

// convert each packet into appropriate format and send it

   

for

(i = 0; i < no_packets; i++){

        can_msg = packet_to_can_msg(tx_pkt_array+i);

         

// insert the prepared packet into the transmission queue

         

// osOK = 0x0

       

if

(!osMutexWait(tx_mutex, osWaitForever)){

            

// put the packet into the queue

            //

wait 5

ms

?

            osMessagePut(tx_CAN_Message_queue, (

uint32_t

)(&can_msg), 5);

            osMutexRelease(tx_mutex);

      }

   }

}

I have tried to insert integers into the message queue and it was successfull.

Please can anybody tell me what I do wrong? Thanks.

#cmsis-rtos #stm32f #free-rtos
5 REPLIES 5
Rob.Riggs
Senior II
Posted on March 23, 2017 at 13:50

Note the differences between Mail Queues and Message Queues.

Posted on March 23, 2017 at 14:42

Hello riggs.rob,

thank you for your reaction. I am not sure whether I understand you

in right manner. Do you mean that I use wrong type of queue for passing

the structures?

Posted on March 23, 2017 at 14:57

Hello riggs.rob,

thank you for your reaction. I am not sure whether I understand you

in right manner. Do you mean that I use wrong type of queue for passing

the structures?

Alan Chambers
Associate II
Posted on March 23, 2017 at 16:39

As riggs.rob indicates, you actually want to use a mail queue. The OS nomenclature is a bit confusing, and changed in CMSIS RTOS v2. I'm using the following template. I don't use the OS macros but declare the necessary structures directly:

template <typename T, uint16_t SIZE>

class MailQueue

{

    public:

        MailQueue()

        {

            for (uint16_t i = 0; i < 4 + SIZE; ++i)

                m_queue[i] = 0;

            

            m_pointers[0] = m_queue;

            m_pointers[1] = m_memory;

            

            m_def.queue_sz = SIZE;

            m_def.item_sz  = sizeof(T);

            m_def.pool     = m_pointers;

            

            m_id = osMailCreate(&m_def, NULL); // , thread id);

            ASSERT(m_id);

        }

        

        void put(const T& message)

        {

            T* mail = static_cast<T*>(osMailAlloc(m_id, 0));

            ASSERT(mail);

            if (mail)

            {

                *mail = message;

                osMailPut(m_id, mail);

            }

        }

        

        void get(T& message)

        {

            osEvent event = osMailGet(m_id, osWaitForever);

            if (event.status == osEventMail)

            {

                T* mail = static_cast<T*>(event.value.p);

                message = *mail;

                osMailFree(m_id, mail);              

            }

        }

    

    private:

        uint32_t           m_queue[4 + SIZE];

        uint32_t           m_memory[3 + ((sizeof(T) + 3) / 4) * SIZE];

        void*              m_pointers[2];

        osMailQDef_t       m_def; // Redundant after osMailCreate() called?

        osMailQId          m_id;

};

hendrikk
Associate III

check this, work pretty fine:

https://www.keil.com/pack/doc/CMSIS/RTOS/html/group__CMSIS__RTOS__Message.html

https://www.keil.com/pack/doc/CMSIS/RTOS/html/group__CMSIS__RTOS__PoolMgmt.html#ga34af5c4f4ab38f4138ea7f1f9ece3a1a

the ST examples in the Cube Repro are very simple!

maybe this is what you need / search for... You can send every structure over the Queue