Skip to main content
ali rostami
Associate III
December 30, 2019
Solved

Order of disabling in `HAL_TIM_IC_Stop_DMA` function

  • December 30, 2019
  • 1 reply
  • 949 views

Here is the function body of `HAL_TIM_IC_Stop_DMA`:

HAL_StatusTypeDef HAL_TIM_IC_Stop_DMA(TIM_HandleTypeDef *htim, uint32_t Channel)
{
 /* Check the parameters */
 assert_param(IS_TIM_CCX_INSTANCE(htim->Instance, Channel));
 assert_param(IS_TIM_DMA_CC_INSTANCE(htim->Instance));
 
 switch (Channel)
 {
 case TIM_CHANNEL_1:
 {
 /* Disable the TIM Capture/Compare 1 DMA request */
 __HAL_TIM_DISABLE_DMA(htim, TIM_DMA_CC1);
 (void)HAL_DMA_Abort_IT(htim->hdma[TIM_DMA_ID_CC1]);
 break;
 }
 
 case TIM_CHANNEL_2:
 {
 /* Disable the TIM Capture/Compare 2 DMA request */
 __HAL_TIM_DISABLE_DMA(htim, TIM_DMA_CC2);
 (void)HAL_DMA_Abort_IT(htim->hdma[TIM_DMA_ID_CC2]);
 break;
 }
 
 case TIM_CHANNEL_3:
 {
 /* Disable the TIM Capture/Compare 3 DMA request */
 __HAL_TIM_DISABLE_DMA(htim, TIM_DMA_CC3);
 (void)HAL_DMA_Abort_IT(htim->hdma[TIM_DMA_ID_CC3]);
 break;
 }
 
 case TIM_CHANNEL_4:
 {
 /* Disable the TIM Capture/Compare 4 DMA request */
 __HAL_TIM_DISABLE_DMA(htim, TIM_DMA_CC4);
 (void)HAL_DMA_Abort_IT(htim->hdma[TIM_DMA_ID_CC4]);
 break;
 }
 
 default:
 break;
 }
 
 /* Disable the Input Capture channel */
 TIM_CCxChannelCmd(htim->Instance, Channel, TIM_CCx_DISABLE);
 
 /* Disable the Peripheral */
 __HAL_TIM_DISABLE(htim);
 
 /* Change the htim state */
 htim->State = HAL_TIM_STATE_READY;
 
 /* Return function status */
 return HAL_OK;
}

My question is why at first it disables the DMA and then disables the input capture channel?

Is the order important?

I have a problem with this order. In my case the input capture triggers another timer every time it captures. so by doing this I have the number of captures. when I used `HAL_TIM_IC_Stop_DMA` function there was a difference between the number of captured data and the counter of the other timer. I found out the problem is because of the order I mentioned. so before calling this function I called `TIM_CCxChannelCmd` and the problem disappeared. But I wonder if it causes any problem.

This topic has been closed for replies.
Best answer by Amel NASRI

More details about the status of this issue can be found in https://github.com/STMicroelectronics/STM32CubeF7/issues/9.

-Amel

1 reply

Amel NASRI
Amel NASRIBest answer
ST Technical Moderator
August 27, 2020

More details about the status of this issue can be found in https://github.com/STMicroelectronics/STM32CubeF7/issues/9.

-Amel

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.