NUCLO.H753ZI, cannot get USB device running
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2023-07-21 1:14 AM
I'd like to activate the user USB on the NUCLO.H753ZI board, as a USB device for serial emulation (CDC)
I use CUBE generated code (basic demo setup for this CPU), the ST-Link USB works and I can debug. I may add, that I have USB working with Cube-code on stm32F-series, so the basics should be there.
In CUBE I set the USB to "Device_only". But when I connect the user USB (CN13) nothing happens, the PC does not recognize a new USB.
The documentation (UM2407 User manual) is a little fuzzy there, but I tried to remove the bridge SB77 , which results in LED 8 (VBUS) only be on when user USB is plugged in, but no other success
Questions:
- Do I overlook sth. obvious?
- The USB is basically OTG. Is there something in the connector or elsewhere to be done
- I found example code but not for this particular CPU. Is there an example around for this CPU, where I can peek?
- Labels:
-
STM32Cube MCU Packages
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2023-09-19 7:07 AM
On my side I did:
* no changes at the eval board
With the STM32CubeMX
at Connectivity USB_OTG_FS
* "Activate_VBUS" disabled
* "Activate_SOF" unhooked
* "VBUS sensing" disabled
at Middleware USB_DEVICE
* "Communication Device Class (Virtual Port Com)" selected
mybe this helps.