2020-04-07 1:14 AM
Hello, I am having problem sendind data to PC with USB. I set the USB_OTG_FS to device only mode and activated the VBUS. I selected Class for FS IP to Communication Device Class (Virtual COM Port). When I try to send data with the simple code below, no data is transmitted to PC:
while(1)
{
//TSA_input_voltage = readVoltageValue(ADC_CHANNEL_5);
memset(USB_String,0x00,255);
StringLength = sprintf(USB_String," USB Voltage in: %d", 5);
CDC_Transmit_FS(USB_String,StringLength);
// HAL_Delay(1000);
}In the debugging window I can see that it gets stuck at :
if (hcdc->TxState != 0){
return USBD_BUSY;
}So USBD is busy all the time. As a side note: I try to debug it by using an oscilloscope and it is clear that USB is initialized correctly. D+ line is high and D- side is low all the time. But that's all. No transmission occurs..
So my question is, what might cause this problem? I believe I am missing some obvious point so I wanted to take opinions. Thanks beforehand.
Solved! Go to Solution.
2020-04-07 4:33 AM
Okay the USB connector was broken. Changed the board and now it works fine.
2020-04-07 4:33 AM
Okay the USB connector was broken. Changed the board and now it works fine.