cancel
Showing results for 
Search instead for 
Did you mean: 

Not getting any data from GNSS-1A using Nucleo STM32F401RE Board.

JLu.1
Associate

Hi,

I use the STM32F401re with GNSS 1A1 module and the sample code from the following GitHub. However, I. However, I cannot read any location from the device and all the tracking seems to be stop. Even I follow the standard procedure of the manual to use the software by official, the reading is still zero. I was wondering is it a broken products or not? So I use another independent GNSS module, the result. For the moment, I couldn't identify the problem. Do you have other customers having the same problem? Or is there any way you can help me?

GitHub:https://github.com/stm32duino/X-NUCLEO-GNSS1A1

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0