STM32F417 + XPT2046 (touch screen)
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2017-02-23 1:57 PM
Hello everyone !
To give you some context : I have a entire project generated by CubeMX on STM32F417, and now, I'm trying to make my touch screen work with it, trough SPI. So far, I can get the IRQ signal, so I detect when I have a touch, but I'm also trying to have the position of the touch, and this is the moment I have a problem.
Every pins are initialized by the code generated by CubeMX, and it's the same for my SPI_Handle.
I saw 'many' examples on the web, most of them they communicate with the functions SPI_I2S_Send/ReceiveData that is normally in the STM32F4XX_StdPeriph_Driver library. But CubeMX didn't generated this library, instead I have the HAL library, with the SPI file, and as I think that CubeMX is not bad, I think that if I don't have the first one, it's because I don't need it. Anyway, I'm trying to make it work with what I have, but I always got the same data, which is not good... Here is the interesting part of my code :
void Touch_GetTouch(uint16_t * xPos, uint16_t * yPos)
{ uint32_t avgX = 0; uint32_t avgY = 0; float calX, calY; TOUCH_CS_RESET; avgX = Touch_Read(CHX); //0x90 avgY = Touch_ReadY(CHY); //0xD0 TOUCH_CS_SET; calX = aX * avgX + bX * avgY + dX; calY = aY * avgX + bY * avgY + dY; *xPos = calX; *yPos = calY;}uint16_t Touch_Read(uint8_t cmd)
{ Touch_Lock(); Touch_Write(cmd); LCD_Delay(10); Touch_Unlock(); return Touch_Read();}uint16_t Touch_Read(void)
{ uint32_t buf; HAL_StatusTypeDef res; uint8_t temp; uint8_t data = 0; /* Wait for SPI3 Tx buffer empty */ while (hspi2.State != HAL_SPI_STATE_READY); res = HAL_SPI_Transmit(&hspi2, &data, 1, 500); if (res == HAL_OK) { while (hspi2.State != HAL_SPI_STATE_READY); res = HAL_SPI_Receive(&hspi2, &temp, 1, 500); } if (res == HAL_OK) { buf=temp<<8; LCD_Delay(1); while (hspi2.State != HAL_SPI_STATE_READY); res = HAL_SPI_Transmit(&hspi2, &data, 1, 500); } if (res == HAL_OK) { while (hspi2.State != HAL_SPI_STATE_READY); res = HAL_SPI_Receive(&hspi2, &temp, 1, 1000); } if (res == HAL_OK) { buf |= temp; buf>>=3; buf&=0xfff; return buf; } return buf;}
void Touch_Write(uint8_t out)
{ while (hspi2.State != HAL_SPI_STATE_READY); HAL_SPI_Transmit(&hspi2, &out, 1, 500); while (hspi2.State != HAL_SPI_STATE_READY); HAL_SPI_Receive(&hspi2, &out, 1, 500);}The Touch_Write and Touch_Read are inspired from some projects I saw, like this one :
http://fabioangeletti.altervista.org/blog/stm32f4-discovery-lcd-touchscreen/
I'm a beginner with the SPI, and most of the STM libraries, so I'm probably missing something stupid and simple, but after two days of trying to find that positions, I can't find out what it is.
Thanks for your help, if you need any infos, no problem !
Antoine
#xpt2046 #stm32f4- Labels:
-
STM32F4 Series