lwIP - TCP echo server in STM32F769-Discovery
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2018-02-22 7:21 AM
Hello,
I am trying to make an example application consisting in a TCP echo server using the RAW from the lwIP stack just to understand how it works. I am using the STM32F769NI - Discovery board as the target which mounts the PHY LAN8742A. I am using the examples in the STM32F7Cube HAL to prepare my project but I am a stuck in the ethernetif.c file.
I can find some examples in the F7Cube HAL using the EVAL boards but those mount a different PHY (DP83848) and also in the F4Cube HAL but with the same problem, different PHY. The fact is that the PHY are different one from another so I can not use the 'hal_conf.h' code with the PHY registers as in those examples. I need to change the use of the registers and the configuration of the interrupts from the PHY.
I am new to the lwIP so I am not sure how to configure the Discovery PHY to use it in the same way as the one in the EVAL boards.
Below I attach the code for the two functions inside the 'eterhnetif.c' file which use those registers (defined in the hal_conf.h) to set up the interrupts needed for this TCP echo application.
/* ethernetif.c file */
...
...
/**
* @brief This function sets the netif link status. * @param netif: the network interface * @retval None */void ethernetif_set_link(struct netif *netif){ uint32_t regvalue = 0; /* Read PHY_MISR*/ HAL_ETH_ReadPHYRegister(&EthHandle, PHY_MISR, ®value); /* Check whether the link interrupt has occurred or not */ if((regvalue & PHY_LINK_INTERRUPT) != (uint16_t)RESET) { /* Read PHY_SR*/ HAL_ETH_ReadPHYRegister(&EthHandle, PHY_SR, ®value); /* Check whether the link is up or down*/ if((regvalue & PHY_LINK_STATUS)!= (uint16_t)RESET) { netif_set_link_up(netif); } else { netif_set_link_down(netif); } }}/* ethernetif.c file */
...
...
...
/**
* @brief In this function, the hardware should be initialized. * Called from ethernetif_init(). * * @param netif the already initialized lwip network interface structure * for this ethernetif */static void low_level_init(struct netif *netif){ uint32_t regvalue = 0; uint8_t macaddress[6]= { MAC_ADDR0, MAC_ADDR1, MAC_ADDR2, MAC_ADDR3, MAC_ADDR4, MAC_ADDR5 }; EthHandle.Instance = ETH; EthHandle.Init.MACAddr = macaddress; EthHandle.Init.AutoNegotiation = ETH_AUTONEGOTIATION_ENABLE; EthHandle.Init.Speed = ETH_SPEED_100M; EthHandle.Init.DuplexMode = ETH_MODE_FULLDUPLEX; EthHandle.Init.MediaInterface = ETH_MEDIA_INTERFACE_MII; EthHandle.Init.RxMode = ETH_RXPOLLING_MODE; EthHandle.Init.ChecksumMode = ETH_CHECKSUM_BY_HARDWARE; EthHandle.Init.PhyAddress = DP83848_PHY_ADDRESS; /* configure ethernet peripheral (GPIOs, clocks, MAC, DMA) */ if (HAL_ETH_Init(&EthHandle) == HAL_OK) { /* Set netif link flag */ netif->flags |= NETIF_FLAG_LINK_UP; } /* Initialize Tx Descriptors list: Chain Mode */ HAL_ETH_DMATxDescListInit(&EthHandle, DMATxDscrTab, &Tx_Buff[0][0], ETH_TXBUFNB); /* Initialize Rx Descriptors list: Chain Mode */ HAL_ETH_DMARxDescListInit(&EthHandle, DMARxDscrTab, &Rx_Buff[0][0], ETH_RXBUFNB); /* set MAC hardware address length */ netif->hwaddr_len = ETH_HWADDR_LEN; /* set MAC hardware address */ netif->hwaddr[0] = MAC_ADDR0; netif->hwaddr[1] = MAC_ADDR1; netif->hwaddr[2] = MAC_ADDR2; netif->hwaddr[3] = MAC_ADDR3; netif->hwaddr[4] = MAC_ADDR4; netif->hwaddr[5] = MAC_ADDR5; /* maximum transfer unit */ netif->mtu = 1500; /* device capabilities */ /* don't set NETIF_FLAG_ETHARP if this device is not an ethernet one */ netif->flags |= NETIF_FLAG_BROADCAST | NETIF_FLAG_ETHARP; /* Enable MAC and DMA transmission and reception */ HAL_ETH_Start(&EthHandle); /**** Configure PHY to generate an interrupt when Eth Link state changes ****/ /* Read Register Configuration */ HAL_ETH_ReadPHYRegister(&EthHandle, PHY_MICR, ®value); regvalue |= (PHY_MICR_INT_EN | PHY_MICR_INT_OE); /* Enable Interrupts */ HAL_ETH_WritePHYRegister(&EthHandle, PHY_MICR, regvalue ); /* Read Register Configuration */ HAL_ETH_ReadPHYRegister(&EthHandle, PHY_MISR, ®value); regvalue |= PHY_MISR_LINK_INT_EN; /* Enable Interrupt on change of link status */ HAL_ETH_WritePHYRegister(&EthHandle, PHY_MISR, regvalue);}Anyone has configured a project to work as TCP echo server using the Discovery board or the PHY mounted on it (LAN8742A)? How can I configure the PHY to work the same way as in the EVAL board application?
Thanks in advanced,
Omar
#ethernet-stm32f7 #stm32f7-hal #phy #tcp/ip- Labels:
-
Ethernet
-
STM32F7 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2018-02-22 7:23 AM
Note that the registers configured in the DP83848 are PHY_SR, PHY_MISR and PHY_MICR.