2024-12-17 9:15 AM
HELLO,
I am working with the LwIP MQTT client(stm32f407) and trying to connect securely to Azure IoT Hub using port 8883. I have enabled secure TLS connections by defining LWIP_ALTCP and LWIP_ALTCP_TLS. However, I am facing a connection reset issue
mqtt_parse_incoming: Remaining length after fixed header: 3
mqtt_parse_incoming: msg_idx: 5, cpy_len: 3, remaining 0
mqtt_tcp_err_cb: TCP error callback: error -15, arg: 0x20004d2c
MQTT: mqtt_connection_cb: Disconnected, reason: 256
code snippet:
#define MQTT_HOST_IP "13.xx.74.xxx"
#define MQTT_HOST_PORT 8883
#define MQTT_USERNAME "xxxxxetestnewhub.azxxxxxxxx/config_test_99/?api-version=2021-04-12" // If required
#define MQTT_PASSWORD "SharedAccessSignature sr=xxxxtestnewhub.azure-devices.net%2Fdevices%2Fconfig_test_99&sig=SawDwVxxxxxxxxxxxxGUHDtuqxaiE%3D&se=1734452908" // If required
const char azure_root_ca[] = "-----BEGIN CERTIFICATE-----\r\n"
"MIIDjjCCAnagAwIBAgIQAzrx5qcRqaC7KGSxHQn65TANBgkqhkiG9w0BAQsFADBh\r\n"
,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,
,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,,
"8rGOmaFvE7FBcf6IKshPECBV1/MUReXgRPTqh5Uykw7+U0b6LJ3/iyK5S9kJRaTe\r\n"
"pLiaWN0bfVKfjllDiIGknibVb63dDcY3fe0Dkhvld1927jyNxF1WW6LZZm6zNTfl\r\n"
"MrY=\r\n"
"-----END CERTIFICATE-----\r\n";
void ConnectionManager() {
err_t err;
uint8_t retryCount = 0;
const uint8_t maxRetries = 5;
mqttclient = mqtt_client_new();
if (mqttclient == NULL) {
printf("Error: Could not create MQTT client\r\n");
return;
}
//generateRandomCharacters(clientId, 16);
strncpy(clientId, "config_test_99", sizeof(clientId) - 1);
clientId[sizeof(clientId) - 1] = '\0'; // Ensure null termination
printf("MQTT Client ID: %s\r\n", clientId);
//mbedtls_debug_set_threshold(4); // mbedtls debug purpose
struct altcp_tls_config *tls_config;
const size_t mbedtls_root_certificate_len = sizeof(azure_root_ca);
tls_config = altcp_tls_create_config_client((const u8_t*)azure_root_ca, mbedtls_root_certificate_len);
if (tls_config == NULL) {
printf("Failed to create TLS configuration.\n");
return;
}
printf("TLS configuration created successfully.\r\n");
memset(&mqttclientInfo, 0, sizeof(mqttclientInfo));
mqttclientInfo.keep_alive = 60;
mqttclientInfo.client_id = clientId;
mqttclientInfo.client_user = MQTT_USERNAME;
mqttclientInfo.client_pass = MQTT_PASSWORD;
mqttclientInfo.tls_config = tls_config;
// Free the TLS configuration after use
//altcp_tls_free_config(tls_config);
broker_ipaddr.addr = ipaddr_addr(MQTT_HOST_IP);
printf("MQTT: connecting to %s\r\n", ipaddr_ntoa(((const ip_addr_t *)&broker_ipaddr)));
while (retryCount < maxRetries) {
if (!mqttConnected) {
printf("MQTT: Attempting to connect to broker...\r\n");
err = mqtt_client_connect(mqttclient, &broker_ipaddr, MQTT_HOST_PORT, mqtt_connection_cb, NULL, &mqttclientInfo);
if (err != ERR_OK) {
printf("MQTT: Connection initiation failed (err: %d). Retrying...\r\n", err);
retryCount++;
osDelay(5000); // Wait before retrying
} else {
printf("MQTT: Connection initiated. Waiting for callback...\r\n");
// Wait for the callback to confirm the connection
uint32_t waitTime = 0;
while (waitTime < 60000 && !mqttConnected) { // 15 seconds timeout
osDelay(100); // Check every 100ms
waitTime += 100;
}
if (mqttConnected) {
printf("MQTT: Successfully connected to broker.\r\n");
// Set the incoming message callbacks
mqtt_set_inpub_callback(mqttclient, mqtt_incoming_publish_cb, mqtt_incoming_data_cb, NULL);
// Subscribe to a topic
mqtt_subscribe_to_topic(mqttclient);
// Publish a test message
mqtt_publish_message(mqttclient);
break;
} else {
printf("MQTT: Connection attempt timed out. Retrying...\r\n");
retryCount++;
}
}
}
osDelay(1000); // Small delay between retries
}
if (!mqttConnected) {
printf("MQTT: Failed to connect after %d attempts.\r\n", retryCount);
}
// Cleanup if needed
mqtt_client_free(mqttclient);
}
Queries for Connecting LWIP MQTT to Azure IoT Hub:
2024-12-17 9:17 PM
Hello,
Any update today?
2024-12-19 8:46 PM
Hello,
Any updates Today?
2024-12-22 9:43 PM
hello,
Any updates?