Skip to main content
VDodi.1
Associate III
September 28, 2023
Solved

Lora Sx1262 integration

Hey,

I want to Integrate with Lora module sx162 with stm32  Board. Can any one Help me ??

This topic has been closed for replies.
Issamos
IssamosBest answer
Super User
September 28, 2023

Hello @VDodi.1 

I think you should use this drive. But I suggest you to use one of the STM32WL MCUs who combine an STM32WL and an sx126x in the same MCU. It has also a firmware that will make it easy to use (configuration, exemples,....).

Best regards.

II

7 replies

VDodi.1
VDodi.1Author
Associate III
September 28, 2023

its Lora 1262.

Issamos
IssamosBest answer
Super User
September 28, 2023

Hello @VDodi.1 

I think you should use this drive. But I suggest you to use one of the STM32WL MCUs who combine an STM32WL and an sx126x in the same MCU. It has also a firmware that will make it easy to use (configuration, exemples,....).

Best regards.

II

VDodi.1
VDodi.1Author
Associate III
October 7, 2023

I don't Find any spi call function ??

 

Tesla DeLorean
Guru
September 28, 2023

Perhaps look at reference schematics and Arduino shields to understand the circuit and connectivity expectations. 

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Associate
September 8, 2025

Hi @Tesla DeLorean,This is ANTONY can you help me to this, I have customised board, I want to connect with the LoRaWAN for uplink and downlink, I have using STM32F103C8T6 MCU chip if you are ready can we discuss 

Tesla DeLorean
Guru
September 9, 2025

Yeah, the F1 is a bit antiquated, most of the LoRa / LRWAN stuff targets the lower-power STM32 families

https://github.com/Saba-abiri/LORA1262

For the Cube add-ons there's https://www.st.com/en/embedded-software/i-cube-lrwan.html

But again not explicitly targeting the F1, so you'll be responsible for doing the porting work. Not a target I'd choose, I migrated the older LRWAN/Semtech libraries, on L1, L0, F4 platforms, for P2P

There might be some forks in Arduino using the radio libraries, but as I recollect these are more LoRa P2P

https://community.st.com/t5/others-hardware-and-software/interfacing-sx1262-lora-module-using-spi-dma/td-p/833871

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..