cancel
Showing results for 
Search instead for 
Did you mean: 

Issues with Code Generation in CubeMX for STM32N657X0H3Q (Non-Secure Mode).

saikumar
Associate III

Hello,

I am new to the STM32N657x0H3Q MCU and trying to generate code from latest CubeMX with the following peripherals enabled:

UART
Ethernet
DCMI
USB
Non-secure region only
However, after generating the code and compiling it in Keli, I am encountering multiple errors. Additionally, CubeMX shows a warning:
"  - Generating AppNS project without AppS, compilation errors maybe generated."

I am trying to understand why this issue occurs.

Is there a strict limitation in this MCU series that requires defining a secure region?
If not, how can I properly generate code with only a non-secure region and avoid these errors?
Also, I am planning to buy the STM32N6570-DK board for my project.

thanks.....

 

0 REPLIES 0