cancel
Showing results for 
Search instead for 
Did you mean: 

Issue in Ethernet and Uart in STM32n6570-DK

MownishBugatha
Associate III

MownishBugatha_0-1770126636796.pngMownishBugatha_1-1770126773759.pngMownishBugatha_2-1770126795188.png

Expected Log using UART :
[BOOT] UART initialized successfully
[BOOT] Starting ThreadX kernel
[NET] NetX Duo initialization started
[NET] IP stack and protocols enabled
[TX] ThreadX kernel running
[NET] NetX application thread running
[NET] Network stack ready
[NET] Static IP: 192.168.1.1

But the it breaks at [NET] NetX application thread running and i have found the following error using debugger and stucked at the error, so need guidance on bring up of Ethernet and perfect log using the UART 

 

I want to send the data from the pc to the STM Board through the ethernet [using] TCP and store the data at some memory so initially i want to bring up the flow and stucked at the error.


 
main.c

/* USER CODE BEGIN Header */
/**
  ******************************************************************************
  * @file           : main.c
  * @brief          : Main program body
  ******************************************************************************
  * @attention
  *
  * Copyright (c) 2026 STMicroelectronics.
  * All rights reserved.
  *
  * This software is licensed under terms that can be found in the LICENSE file
  * in the root directory of this software component.
  *
  ******************************************************************************
  */
/* USER CODE END Header */

/* Includes ------------------------------------------------------------------*/
#include "app_threadx.h"
#include "main.h"
#include "string.h"

/* Private variables ---------------------------------------------------------*/
#if defined ( __ICCARM__ )
#pragma location=0x34100000
ETH_DMADescTypeDef  DMARxDscrTab[ETH_DMA_RX_CH_CNT][ETH_RX_DESC_CNT];
#pragma location=0x341000C0
ETH_DMADescTypeDef  DMATxDscrTab[ETH_DMA_TX_CH_CNT][ETH_TX_DESC_CNT];

#elif defined ( __CC_ARM )

__attribute__((at(0x34100000))) ETH_DMADescTypeDef  DMARxDscrTab[ETH_DMA_RX_CH_CNT][ETH_RX_DESC_CNT];
__attribute__((at(0x341000C0))) ETH_DMADescTypeDef  DMATxDscrTab[ETH_DMA_TX_CH_CNT][ETH_TX_DESC_CNT];

#elif defined ( __GNUC__ )

ETH_DMADescTypeDef DMARxDscrTab[ETH_DMA_RX_CH_CNT][ETH_RX_DESC_CNT]
__attribute__((section(".RxDecripSection")));
ETH_DMADescTypeDef DMATxDscrTab[ETH_DMA_TX_CH_CNT][ETH_TX_DESC_CNT]
__attribute__((section(".TxDecripSection")));
#endif

ETH_TxPacketConfig TxConfig;
ETH_HandleTypeDef heth1;
UART_HandleTypeDef huart1;

/* Private function prototypes -----------------------------------------------*/
static void MX_GPIO_Init(void);
static void MX_ETH1_Init(void);
static void MX_USART1_UART_Init(void);
void SystemClock_Config(void);
void Error_Handler(void);

/* USER CODE BEGIN 0 */
/* USER CODE END 0 */

int main(void)
{
  /* ------------------------------------------------------------------
   * 1. Enable caches FIRST (required for ETH / DMA)
   * ------------------------------------------------------------------ */
  SCB_EnableICache();
  SCB_EnableDCache();

  /* ------------------------------------------------------------------
   * 2. HAL + clocks
   * ------------------------------------------------------------------ */
  HAL_Init();
  SystemClock_Config();

  /* ------------------------------------------------------------------
   * 3. Low-level peripherals (NO RTOS here)
   * ------------------------------------------------------------------ */
  MX_GPIO_Init();
  MX_ETH1_Init();          /* ETH HAL init only (NetX will handle runtime) */
  MX_USART1_UART_Init();

  /* ------------------------------------------------------------------
   * 4. Pre-RTOS UART sanity logs (blocking, short, safe)
   * ------------------------------------------------------------------ */
  const char msg1[] = "[BOOT] UART initialized successfully\r\n";
  const char msg2[] = "[BOOT] Starting ThreadX kernel\r\n";

  HAL_UART_Transmit(&huart1, (uint8_t *)msg1, sizeof(msg1) - 1, 100);
  HAL_UART_Transmit(&huart1, (uint8_t *)msg2, sizeof(msg2) - 1, 100);

  /* ------------------------------------------------------------------
   * 5. Start ThreadX (never returns)
   * ------------------------------------------------------------------ */
  MX_ThreadX_Init();

  /* ------------------------------------------------------------------
   * 6. Should never reach here
   * ------------------------------------------------------------------ */
  while (1)
  {
  }
}

/* ========================= Peripheral init code ========================== */
/* (UNCHANGED — CubeMX generated)                                           */
/* ========================================================================= */

static void MX_ETH1_Init(void)
{
  static uint8_t MACAddr[6];

  memset(&TxConfig, 0 , sizeof(ETH_TxPacketConfig));
  TxConfig.Attributes = ETH_TX_PACKETS_FEATURES_CSUM | ETH_TX_PACKETS_FEATURES_CRCPAD;
  TxConfig.ChecksumCtrl = ETH_CHECKSUM_IPHDR_PAYLOAD_INSERT_PHDR_CALC;
  TxConfig.CRCPadCtrl = ETH_CRC_PAD_INSERT;

  heth1.Instance = ETH1;
  MACAddr[0] = 0x00;
  MACAddr[1] = 0x80;
  MACAddr[2] = 0xE1;
  MACAddr[3] = 0x00;
  MACAddr[4] = 0x00;
  MACAddr[5] = 0x00;
  heth1.Init.MACAddr = &MACAddr[0];
  heth1.Init.MediaInterface = HAL_ETH_RGMII_MODE;

  for (int ch = 0; ch < ETH_DMA_CH_CNT; ch++)
  {
    heth1.Init.TxDesc[ch] = DMATxDscrTab[ch];
    heth1.Init.RxDesc[ch] = DMARxDscrTab[ch];
  }

  heth1.Init.RxBuffLen = 1536;

  if (HAL_ETH_Init(&heth1) != HAL_OK)
  {
    Error_Handler();
  }
}

static void MX_USART1_UART_Init(void)
{
  huart1.Instance = USART1;
  huart1.Init.BaudRate = 115200;
  huart1.Init.WordLength = UART_WORDLENGTH_8B;
  huart1.Init.StopBits = UART_STOPBITS_1;
  huart1.Init.Parity = UART_PARITY_NONE;
  huart1.Init.Mode = UART_MODE_TX_RX;
  huart1.Init.HwFlowCtl = UART_HWCONTROL_NONE;
  huart1.Init.OverSampling = UART_OVERSAMPLING_16;
  huart1.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE;
  huart1.Init.ClockPrescaler = UART_PRESCALER_DIV1;
  huart1.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT;

  if (HAL_UART_Init(&huart1) != HAL_OK)
  {
    Error_Handler();
  }

  HAL_UARTEx_SetTxFifoThreshold(&huart1, UART_TXFIFO_THRESHOLD_1_8);
  HAL_UARTEx_SetRxFifoThreshold(&huart1, UART_RXFIFO_THRESHOLD_1_8);
  HAL_UARTEx_DisableFifoMode(&huart1);
}
static void MX_GPIO_Init(void)
{
  /* USER CODE BEGIN MX_GPIO_Init_1 */

  /* USER CODE END MX_GPIO_Init_1 */

  /* GPIO Ports Clock Enable */
  __HAL_RCC_GPIOD_CLK_ENABLE();
  __HAL_RCC_GPIOE_CLK_ENABLE();
  __HAL_RCC_GPIOF_CLK_ENABLE();
  __HAL_RCC_GPIOG_CLK_ENABLE();

  /* USER CODE BEGIN MX_GPIO_Init_2 */

  /* USER CODE END MX_GPIO_Init_2 */
}

/* USER CODE BEGIN 4 */
void SystemClock_Config(void)
{
  RCC_OscInitTypeDef RCC_OscInitStruct = {0};
  RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

  if (HAL_PWREx_ConfigSupply(PWR_EXTERNAL_SOURCE_SUPPLY) != HAL_OK)
  {
    Error_Handler();
  }

  if (HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE1) != HAL_OK)
  {
    Error_Handler();
  }

  /* Enable HSI */
  RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
  RCC_OscInitStruct.HSIState = RCC_HSI_ON;
  RCC_OscInitStruct.HSIDiv = RCC_HSI_DIV1;
  RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
  RCC_OscInitStruct.PLL1.PLLState = RCC_PLL_NONE;
  RCC_OscInitStruct.PLL2.PLLState = RCC_PLL_NONE;
  RCC_OscInitStruct.PLL3.PLLState = RCC_PLL_NONE;
  RCC_OscInitStruct.PLL4.PLLState = RCC_PLL_NONE;

  if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
  {
    Error_Handler();
  }

  HAL_RCC_GetClockConfig(&RCC_ClkInitStruct);
  if ((RCC_ClkInitStruct.CPUCLKSource == RCC_CPUCLKSOURCE_IC1) ||
      (RCC_ClkInitStruct.SYSCLKSource == RCC_SYSCLKSOURCE_IC2_IC6_IC11))
  {
    RCC_ClkInitStruct.ClockType = (RCC_CLOCKTYPE_CPUCLK | RCC_CLOCKTYPE_SYSCLK);
    RCC_ClkInitStruct.CPUCLKSource = RCC_CPUCLKSOURCE_HSI;
    RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI;

    if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct) != HAL_OK)
    {
      Error_Handler();
    }
  }

  RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_NONE;
  RCC_OscInitStruct.PLL1.PLLState = RCC_PLL_ON;
  RCC_OscInitStruct.PLL1.PLLSource = RCC_PLLSOURCE_HSI;
  RCC_OscInitStruct.PLL1.PLLM = 4;
  RCC_OscInitStruct.PLL1.PLLN = 75;
  RCC_OscInitStruct.PLL1.PLLFractional = 0;
  RCC_OscInitStruct.PLL1.PLLP1 = 1;
  RCC_OscInitStruct.PLL1.PLLP2 = 1;

  if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
  {
    Error_Handler();
  }

  RCC_ClkInitStruct.ClockType =
      RCC_CLOCKTYPE_CPUCLK | RCC_CLOCKTYPE_HCLK |
      RCC_CLOCKTYPE_SYSCLK | RCC_CLOCKTYPE_PCLK1 |
      RCC_CLOCKTYPE_PCLK2 | RCC_CLOCKTYPE_PCLK4 |
      RCC_CLOCKTYPE_PCLK5;

  RCC_ClkInitStruct.CPUCLKSource = RCC_CPUCLKSOURCE_IC1;
  RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_IC2_IC6_IC11;

  /* 🔑 IMPORTANT LINE */
  RCC_ClkInitStruct.AHBCLKDivider = RCC_HCLK_DIV2;

  RCC_ClkInitStruct.APB1CLKDivider = RCC_APB1_DIV1;
  RCC_ClkInitStruct.APB2CLKDivider = RCC_APB2_DIV1;
  RCC_ClkInitStruct.APB4CLKDivider = RCC_APB4_DIV1;
  RCC_ClkInitStruct.APB5CLKDivider = RCC_APB5_DIV1;

  RCC_ClkInitStruct.IC1Selection.ClockSelection = RCC_ICCLKSOURCE_PLL1;
  RCC_ClkInitStruct.IC1Selection.ClockDivider = 2;
  RCC_ClkInitStruct.IC2Selection.ClockSelection = RCC_ICCLKSOURCE_PLL1;
  RCC_ClkInitStruct.IC2Selection.ClockDivider = 3;
  RCC_ClkInitStruct.IC6Selection.ClockSelection = RCC_ICCLKSOURCE_PLL1;
  RCC_ClkInitStruct.IC6Selection.ClockDivider = 4;
  RCC_ClkInitStruct.IC11Selection.ClockSelection = RCC_ICCLKSOURCE_PLL1;
  RCC_ClkInitStruct.IC11Selection.ClockDivider = 3;

  if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct) != HAL_OK)
  {
    Error_Handler();
  }
}
/* USER CODE END 4 */

/**
  * @brief  This function is executed in case of error occurrence.
  * @retval None
  */
void Error_Handler(void)
{
  /* USER CODE BEGIN Error_Handler_Debug */
  /* User can add his own implementation to report the HAL error return state */
  __disable_irq();
  while (1)
  {
  }
  /* USER CODE END Error_Handler_Debug */
}
#ifdef USE_FULL_ASSERT
/**
  * @brief  Reports the name of the source file and the source line number
  *         where the assert_param error has occurred.
  * @PAram  file: pointer to the source file name
  * @PAram  line: assert_param error line source number
  * @retval None
  */
void assert_failed(uint8_t *file, uint32_t line)
{
  /* USER CODE BEGIN 6 */
  /* User can add his own implementation to report the file name and line number,
     ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
  /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */

 

app_netxduo.c

#include "app_netxduo.h"
#include "stm32n6xx_hal.h"
#include "main.h"
#include <stdio.h>
#include <string.h>

/* NetX objects -------------------------------------------------------------*/
TX_THREAD      NxAppThread;
NX_PACKET_POOL NxAppPool;
NX_IP          NetXDuoEthIpInstance;
TX_MUTEX       uart_mutex;

/* Private prototypes -------------------------------------------------------*/
static VOID App_Main_Thread_Entry(ULONG thread_input);

extern UART_HandleTypeDef huart1;

/**
  * @brief  NetXDuo Initialization
  */
UINT MX_NetXDuo_Init(VOID *memory_ptr)
{
    TX_BYTE_POOL *byte_pool = (TX_BYTE_POOL *)memory_ptr;
    UCHAR *pointer;

    /* ---- UART mutex (MUST be created before any RTOS print) ---- */
    tx_mutex_create(&uart_mutex, "UART Mutex", TX_INHERIT);

    tx_mutex_get(&uart_mutex, TX_WAIT_FOREVER);
    HAL_UART_Transmit(&huart1,
        (uint8_t *)"[NET] NetX Duo initialization started\r\n",
        sizeof("[NET] NetX Duo initialization started\r\n") - 1,
        HAL_MAX_DELAY);
    tx_mutex_put(&uart_mutex);

    /* ---- NetX system ---- */
    nx_system_initialize();

    /* ---- Packet pool ---- */
    tx_byte_allocate(byte_pool, (VOID **)&pointer,
                     NX_APP_PACKET_POOL_SIZE, TX_NO_WAIT);

    nx_packet_pool_create(&NxAppPool,
                          "NetX Packet Pool",
                          DEFAULT_PAYLOAD_SIZE,
                          pointer,
                          NX_APP_PACKET_POOL_SIZE);

    /* ---- IP instance ---- */
    tx_byte_allocate(byte_pool, (VOID **)&pointer,
                     Nx_IP_INSTANCE_THREAD_SIZE, TX_NO_WAIT);

    nx_ip_create(&NetXDuoEthIpInstance,
                 "NetX IP",
                 NX_APP_DEFAULT_IP_ADDRESS,
                 NX_APP_DEFAULT_NET_MASK,
                 &NxAppPool,
                 nx_stm32_eth_driver,
                 pointer,
                 Nx_IP_INSTANCE_THREAD_SIZE,
                 NX_APP_INSTANCE_PRIORITY);

    /* ---- Enable protocols ---- */
    static UCHAR arp_cache[DEFAULT_ARP_CACHE_SIZE];
    nx_arp_enable(&NetXDuoEthIpInstance, arp_cache, DEFAULT_ARP_CACHE_SIZE);
    nx_icmp_enable(&NetXDuoEthIpInstance);
    nx_udp_enable(&NetXDuoEthIpInstance);
    nx_tcp_enable(&NetXDuoEthIpInstance);

    tx_mutex_get(&uart_mutex, TX_WAIT_FOREVER);
    HAL_UART_Transmit(&huart1,
        (uint8_t *)"[NET] IP stack and protocols enabled\r\n",
        sizeof("[NET] IP stack and protocols enabled\r\n") - 1,
        HAL_MAX_DELAY);
    tx_mutex_put(&uart_mutex);

    /* ---- Application thread ---- */
    tx_byte_allocate(byte_pool, (VOID **)&pointer,
                     NX_APP_THREAD_STACK_SIZE, TX_NO_WAIT);

    tx_thread_create(&NxAppThread,
                     "NetX App Thread",
                     App_Main_Thread_Entry,
                     0,
                     pointer,
                     NX_APP_THREAD_STACK_SIZE,
                     NX_APP_THREAD_PRIORITY,
                     NX_APP_THREAD_PRIORITY,
                     TX_NO_TIME_SLICE,
                     TX_AUTO_START);

    return NX_SUCCESS;
}

/**
  * @brief  NetX application main thread
  */
static VOID App_Main_Thread_Entry(ULONG thread_input)
{
    ULONG ip, mask, status;
    char msg[64];

    (void)thread_input;

    tx_mutex_get(&uart_mutex, TX_WAIT_FOREVER);
    HAL_UART_Transmit(&huart1,
        (uint8_t *)"[NET] NetX application thread running\r\n",
        sizeof("[NET] NetX application thread running\r\n") - 1,
        HAL_MAX_DELAY);
    tx_mutex_put(&uart_mutex);

    /* ---- Wait for Ethernet link ---- */
    do
    {
        nx_ip_status_check(&NetXDuoEthIpInstance,
                           NX_IP_LINK_ENABLED,
                           &status,
                           TX_NO_WAIT);
        tx_thread_sleep(TX_TIMER_TICKS_PER_SECOND / 2);
    } while (!(status & NX_IP_LINK_ENABLED));

    tx_mutex_get(&uart_mutex, TX_WAIT_FOREVER);
    HAL_UART_Transmit(&huart1,
        (uint8_t *)"[NET] Ethernet link UP\r\n",
        sizeof("[NET] Ethernet link UP\r\n") - 1,
        HAL_MAX_DELAY);
    tx_mutex_put(&uart_mutex);

    /* ---- Static gateway ---- */
    nx_ip_gateway_address_set(&NetXDuoEthIpInstance,
                              NX_APP_DEFAULT_GATEWAY_ADDRESS);

    /* ---- Read assigned IP ---- */
    nx_ip_address_get(&NetXDuoEthIpInstance, &ip, &mask);

    sprintf(msg,
            "[NET] Static IP: %lu.%lu.%lu.%lu\r\n",
            (ip >> 24) & 0xFF,
            (ip >> 16) & 0xFF,
            (ip >> 8) & 0xFF,
            ip & 0xFF);

    tx_mutex_get(&uart_mutex, TX_WAIT_FOREVER);
    HAL_UART_Transmit(&huart1,
        (uint8_t *)msg,
        strlen(msg),
        HAL_MAX_DELAY);
    tx_mutex_put(&uart_mutex);

    /* ---- Idle ---- */
    while (1)
    {
        tx_thread_sleep(TX_TIMER_TICKS_PER_SECOND);
    }
}

 

app_thread.c

/* Includes ------------------------------------------------------------------*/
#include "app_threadx.h"
#include "stm32n6xx_hal.h"
#include "main.h"
#include "tx_api.h"
#include <string.h>

/* Private defines -----------------------------------------------------------*/
#define UART_THREAD_STACK_SIZE   1024
#define UART_THREAD_PRIORITY     15

/* Private variables ---------------------------------------------------------*/
static TX_THREAD uart_thread;
static ULONG uart_thread_stack[UART_THREAD_STACK_SIZE / sizeof(ULONG)];

/* External variables --------------------------------------------------------*/
extern UART_HandleTypeDef huart1;
extern TX_MUTEX uart_mutex;

/* Private function prototypes -----------------------------------------------*/
static void uart_thread_entry(ULONG thread_input);

/**
  * @brief  Application ThreadX Initialization.
  */
UINT App_ThreadX_Init(VOID *memory_ptr)
{
  (void)memory_ptr;

  /* Create UART debug thread */
  if (tx_thread_create(&uart_thread,
                       "UART Debug Thread",
                       uart_thread_entry,
                       0,
                       uart_thread_stack,
                       sizeof(uart_thread_stack),
                       UART_THREAD_PRIORITY,
                       UART_THREAD_PRIORITY,
                       TX_NO_TIME_SLICE,
                       TX_AUTO_START) != TX_SUCCESS)
  {
    return TX_THREAD_ERROR;
  }

  return TX_SUCCESS;
}

/**
  * @brief  ThreadX Kernel Start
  */
void MX_ThreadX_Init(void)
{
  tx_kernel_enter();
}

/**
  * @brief  UART debug / system status thread
  */
static void uart_thread_entry(ULONG thread_input)
{
  (void)(thread_input);

  /* ---- ONE-TIME RTOS START LOG ---- */
  tx_mutex_get(&uart_mutex, TX_WAIT_FOREVER);
  HAL_UART_Transmit(&huart1,
                    (uint8_t *)"[TX] ThreadX kernel running\r\n",
                    sizeof("[TX] ThreadX kernel running\r\n") - 1,
                    HAL_MAX_DELAY);
  tx_mutex_put(&uart_mutex);

  /* ---- Thread stays alive, but silent ---- */
  while (1)
  {
    tx_thread_sleep(TX_TIMER_TICKS_PER_SECOND);
  }
}

 



0 REPLIES 0