2022-09-13 08:52 PM
AT%CEER?<CR>
<CR><LF>
%CEER: 1,"NAS-EMM","ATTACH","REJECT",#15,NO_SUITABLE_CELLS_IN_TRACKING_AREA<CR><LF>
<CR><LF>
OK<CR><LF>
Here is the modem configuration:
Cellular Service Infos
Modem state : 4 (Modem registered on network)
Signal Quality : 0
Signal level(dBm) : 0
Operator name :
IMEI : 351521100639475
Manuf name : Murata Manufacturing Co.
Model : LBAD0XX1SC-DM
Revision : RK_03_00_00_00_04121_001
Serial Number : 351521100639475
ICCID : 8944477300000104512
IMSI : 208090022802391
Network bearer (AcT) : 0 (GSM)
IP address : 0.0.0.0
Cellular Service Task State
Current State : WAITING_FOR_NETWORK_STATUS_STATE
Sim Selected : EXTERNAL MODEM SLOT > SIM initialized and ready
All sim information :
- Sim REMOVABLE SLOT : SIM error - too many error rsp during init
APN :
APN username :
APN password :
APN is sent to modem
- Sim EXTERNAL MODEM SLOT : SIM initialized and ready
APN : iot.truphone.com
APN username :
APN password :
APN is sent to modem
Cellular Service Task Config
Sim Slot : 0 (REMOVABLE SLOT)
APN : ""
CID : 1
username :
password :
Sim Slot : 1 (EXTERNAL MODEM SLOT)
APN : "iot.truphone.com"
CID : 1
username :
password :
Attachment timeout : 180000 ms
nfmc mode : Not active
Network register mode: 0 = Auto
Access techno present: Not present
$>at at%nwoper="TRUPHONE"
ATParser:*** SEND (size=21) ***
at%nwoper="TRUPHONE"<CR>
<CR><LF>
OK<CR><LF>
I hope someone can help me to resolve this issue.
Thank you all.
2022-10-24 06:19 PM
Same here, also gave up trying Truphone after a while and used Telstra SIM card instead.
2024-01-06 12:38 AM
Hi Desh,
I'm also getting started with the BL462E-CELL1. Did your BL462E-CELL1 come with "RK_03_00_00_00_04121_001" as the default modem firmware version? Or you had to update it?
I'm having a challenge of updating the modem firmware version to "RK_03_00_00_00_04121_001" so as to be compliant with the latest X-CUBECELLULAR v7.1.0.
Thanks.
2024-02-12 08:21 AM
With consultation from the muRata support team, the modem factory FW version (RK_03_00_00_00_11851_001) which was pre-installed was compliant with the X-CUBECELLULAR v7.1.0. So, I tested it, and it worked great.