2019-04-05 4:11 AM
The hardware pin has been set high and the boot address in register is same as ST programmed value. Baud rate is set to 9600.
2019-04-05 8:06 AM
Does it function otherwise?
What board?
Is it using a supported USART and pins?
2019-04-05 9:00 AM
Is bootloader triggered by configuring the BOOT0 pin which level is latched at reset rising edge?
Maybe do this manually, then use the USART?
2019-04-08 9:21 PM
@Community member
Yes the board functions otherwise. We have designed our own board. PA9 and PA10 have been used for USART and they are supported.