cancel
Showing results for 
Search instead for 
Did you mean: 

How to use the line level input of a STM32H735G-DK with LiveTune

euanbrown
Associate

I am using the STM32H735G-DK development kit to evaluate the LiveTune audio kit capabilities.

When connecting to the dev board it shows several audio input source but does not show one for the Line Level input on connector CN11.

How do I use the Line Level Input with the LiveTune software?

Only options shown are

  • SysIn-MicroPDM
  • SysIn-Microphones
  • SysIn-USB
0 REPLIES 0