Skip to main content
JBias
Associate III
January 20, 2025
Question

Hard Fault with external memory bootloader STM32H7S3L8H6

  • January 20, 2025
  • 1 reply
  • 1108 views

While trying to implement the stm32h7s_workshop I'm always getting hard faults.

JBias_0-1737348584949.png

Seems straight forward. I checked to see that the external FLASH verifies against the appli.elf and I made sure to debug with the boot 1st then the appli.

Here's what I see in the CubeProgrammer

JBias_1-1737348803563.png

Could this be due to an alignment issue? 

The fault comes just at the point where it is going to jump to the appli

 

 

This topic has been closed for replies.

1 reply

ST Employee
January 22, 2025

Hello @JBias ,

If you followed the workshop steps correctly it is highly unlikely you get into a hardfault please review the steps and check if you have correct MPU configuration or try to compare you generated project with the available example in GitHub of in Cube Firmware package to see what you are missing exactly.
Regards 

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.