cancel
Showing results for 
Search instead for 
Did you mean: 

How to receive USB resume signal from host when STM32F407 send remote wakeup signal

Harry0709
Associate

Environment:

STM32F407VGTX 

USB HID mouse, Full Speed

Problem:

Hi, I’m using a STM32F407VGTX board. I send a USB remote wakeup signal to the host and then try to receive a resume signal from the host. The STM32 board can wake up the host (bringing it to the login screen), but it cannot trigger the USB_OTG_GINTSTS_WKUINT interrupt. I have already configured my STM32 board as a HID mouse. However, if I use a real mouse instead, it can wake up the host and successfully trigger the USB_OTG_GINTSTS_WKUINT interrupt. Is there any suggestion or workaround for this problem?

 

void usb_remote_wakeup()
{
    if (hUsbDeviceFS.dev_remote_wakeup == 1)
    {
        __HAL_PCD_UNGATE_PHYCLOCK(&hpcd_USB_OTG_FS);
        HAL_PCD_ActivateRemoteWakeup(&hpcd_USB_OTG_FS);
        HAL_Delay(5);
        HAL_PCD_DeActivateRemoteWakeup(&hpcd_USB_OTG_FS);
    }
}

 

1 REPLY 1
T_Hamdi
ST Employee

Hello @Harry0709 

 

You can refer to the USB HID application available in the STM32CubeF4 firmware:

HID application support remote wakeup 

If you are not able to trigger the USB_OTG_GINTSTS_WKUINT interrupt, you can share with me how you are trying to trigger it, and I will help you

best regards,

hamdi

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
Hamdi Teyeb