2024-02-28 06:51 AM - last edited on 2025-02-20 12:59 AM by FBL
Hello Everybody,
I sucessfully included the X-CUBE-TCPP software expanison onta a NUCLEO-G071RB Board.
After some inital tests we decided to switch to the NUCLEO-G0B1RE Board for more flash as the Getting Started PDF (https://www.st.com/resource/en/user_manual/um2902-getting-started-with-the-usb-typec-software-expansion-for-stm32cube-stmicroelectronics.pdf) said that it would be possible to port the software to this chip.
I did the instructions (https://wiki.st.com/stm32mcu/wiki/STM32StepByStep:Getting_started_with_USB-Power_Delivery_Dual_Role) again, but i discovered that it wouldn't work now.AS it seems the Task won't start
I tried to connect the board agin to the stm32CubeMonitor with no suscess. I attached the traces file. Also the RTOS tasks seems not to start without a reason.
What do I have to change to get it running on the G0B1RE Board?
Thanks in advance.
2024-02-29 06:16 AM
Hello @VH
I tried to connect the board again to the stm32CubeMonitor with no success. I attached the traces file. Also, the RTOS tasks seems not to start without a reason.
First, let's check your hardware configuration: CN4 should be shorten 1-2, 3-4 for connection with STM32CubeMonUCPD. If this is already done, we suggest you checking your flash configuration.
I was wondering which toolchain is used?
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-02-29 11:48 AM
Hello @VH ,
There has been a case created to resolve this question and we will be reaching out to you directly.
Regards,
Roger