How to implement 2 virtual com ports on 1 USB interface
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2016-12-28 5:39 AM
Posted on December 28, 2016 at 14:39
Hi,
I am using CubeMx in order to generate startup code for the USB virtual com port device. It works fine. But I need to implement 2 virtual com ports on 1 USB interface. I cant seem to find any source of information how to do it. I would appreciate all
Please any one explain were I need to modify.
I modified
USB Standard Device Descriptor file IADClasscode Document but still is not working.
device class to-0xEF, /*bDeviceClass*/
Device sub class to- 0x02, /*bDeviceSubClass*/ Device Protocol- 0x01, /*bDeviceProtocol*/#if defined ( __ICCARM__ ) /*!< IAR Compiler */
#pragma data_alignment=4
#endif
/* USB Standard Device Descriptor */
__ALIGN_BEGIN uint8_t USBD_FS_DeviceDesc[USB_LEN_DEV_DESC] __ALIGN_END =
{
0x12, /*bLength */
USB_DESC_TYPE_DEVICE, /*bDescriptorType*/
#if (USBD_LPM_ENABLED == 1)
0x01, /*bcdUSB */ /* changed to USB version 2.01
in order to support LPM L1 suspend
resume test of USBCV3.0*/
#else
0x00, /* bcdUSB */
#endif
0x02,
0xEF, /*bDeviceClass*/
0x02, /*bDeviceSubClass*/
0x01, /*bDeviceProtocol*/
USB_MAX_EP0_SIZE, /*bMaxPacketSize*/
LOBYTE(USBD_VID), /*idVendor*/
HIBYTE(USBD_VID), /*idVendor*/
LOBYTE(USBD_PID_FS), /*idVendor*/
HIBYTE(USBD_PID_FS), /*idVendor*/
0x00, /*bcdDevice rel. 2.00*/
0x02,
USBD_IDX_MFC_STR, /*Index of manufacturer string*/
USBD_IDX_PRODUCT_STR, /*Index of product string*/
USBD_IDX_SERIAL_STR, /*Index of serial number string*/
USBD_MAX_NUM_CONFIGURATION /*bNumConfigurations*/
} ;�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
#usb-cdc
Labels:
- Labels:
-
USB
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2016-12-30 7:32 AM
Posted on December 30, 2016 at 16:32
Dear
G.Vijay
,You may refer to this
and presentationwhich can help you on USB VCP device topic.Happy New Year
Imen
When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Thanks
Imen