2021-03-10 12:33 AM
Hello,
I am trying to write data in .txt file on a USB pendrive at a certain frequency (in the while 1 loop) using STM32L496ZG as the USB host in the Mass Storage Class (MSC) configuration.
I succeded writing to the .txt file in the first iteration, but after I can't access the USB pendrive anymore. I investigated the matter and I found out that when accessing the USB pendrive in the first iteration, the MSC_Handle->State is put to MSC_IDLE (see code below).
static USBH_StatusTypeDef USBH_MSC_Process(USBH_HandleTypeDef *phost)
{
MSC_HandleTypeDef *MSC_Handle = (MSC_HandleTypeDef *) phost->pActiveClass->pData;
USBH_StatusTypeDef error = USBH_BUSY;
USBH_StatusTypeDef scsi_status = USBH_BUSY;
USBH_StatusTypeDef ready_status = USBH_BUSY;
switch (MSC_Handle->state)
{
case MSC_INIT:
if (MSC_Handle->current_lun < MSC_Handle->max_lun)
{
.... // initialization of the MSC
}
//MSC initialization finished
else // if (MSC_Handle->current_lun >= MSC_Handle->max_lun) where max_lun =1
{
MSC_Handle->current_lun = 0U;
MSC_Handle->state = MSC_IDLE; //MSC put to IDLE
phost->pUser(phost, HOST_USER_CLASS_ACTIVE); //access to the USB
}
break;
In the MSC_IDLE state, we can't access anymore the USB pendrive.
case MSC_IDLE:
error = USBH_OK;
break;I tried finding where to put the MSC_Handle->State back to MSC_INIT but with no success.
May anyone has a clue to share?
Tell me if more details, on what I did, is needed.
Thanks in advance for your help