How to Enable GPIO External Interrupts STM32F30x_StdPeriph_Driver
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-01-29 12:53 AM
Hi I'm working on a project where I need to enable external GPIO interrupts on the STM32F303 discovery board. I've looked up several examples online, but can't seem to get in to work. I'm using theSTM32F30x_StdPeriph_Driver. I see in several examples that GPIO_MODE_IT_RISING is used as the GPIO pin mode for interrupts, but this is a HAL library thing and not present in the StdPeriph.
I am using EXTI_LINE12 with GPIO PB12 in input pullup mode with trigger on the rising edge, vector isEXTI15_10_IRQn. Please let me know if you see anything I am doing wrong, I am at a loss at this point. Code is included below, thanks!
Function where I instantiate GPIO and interrupt (called in main):
static void GPIO_InputInit(void){
GPIO_InitTypeDef GPIO_InitStructure;
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOE, ENABLE);
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOB, ENABLE);
RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOD, ENABLE);
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_15 | GPIO_Pin_14;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN;
//GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;
GPIO_Init(GPIOE, &GPIO_InitStructure);
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_2 | GPIO_Pin_10 | GPIO_Pin_11 | GPIO_Pin_12 | GPIO_Pin_13 | GPIO_Pin_14 | GPIO_Pin_15; //GPIO_Pin_12
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;
GPIO_Init(GPIOB, &GPIO_InitStructure);
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_15;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;
GPIO_Init(GPIOD, &GPIO_InitStructure);
EXTI_InitTypeDef EXTI_InitStruct;
NVIC_InitTypeDef NVIC_InitStruct;
/* Tell system that you will use PB12 for EXTI_Line12 */
SYSCFG_EXTILineConfig(EXTI_PortSourceGPIOB, EXTI_PinSource12);
/* PB12 is connected to EXTI_Line12 */
EXTI_InitStruct.EXTI_Line = EXTI_Line12;
/* Enable interrupt */
EXTI_InitStruct.EXTI_LineCmd = ENABLE;
/* Interrupt mode */
EXTI_InitStruct.EXTI_Mode = EXTI_Mode_Interrupt;
/* Triggers on rising and falling edge */
EXTI_InitStruct.EXTI_Trigger = EXTI_Trigger_Rising;
/* Add to EXTI */
EXTI_Init(&EXTI_InitStruct);
/* Add IRQ vector to NVIC */
/* PB12 is connected to EXTI_Line12, which has EXTI15_10_IRQn vector */
NVIC_InitStruct.NVIC_IRQChannel = EXTI15_10_IRQn;
/* Set priority */
NVIC_InitStruct.NVIC_IRQChannelPreemptionPriority = 0x00;
/* Set sub priority */
NVIC_InitStruct.NVIC_IRQChannelSubPriority = 0x01;
/* Enable interrupt */
NVIC_InitStruct.NVIC_IRQChannelCmd = ENABLE;
/* Add to NVIC */
NVIC_Init(&NVIC_InitStruct);
}�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
Interrupt Function:
void EXTI15_10_IRQHandler(void) {
interruptCounter++;
interruptFlag = 1;
if (EXTI_GetITStatus(EXTI_Line12) != RESET) {
envStage = 1;
EXTI_ClearITPendingBit(EXTI_Line12);
}
}�?�?�?�?�?�?�?�?
#standard-peripheral #gpio #exti #interrupt #stm32f303
- Labels:
-
GPIO-EXTI
-
Interrupt
-
SPL
-
STM32F3 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-01-30 7:24 AM
Hi
Palaima.Emmett
,Have a look to this example :STM32F30x_DSP_StdPeriph_Lib_V1.2.3\Projects\STM32F30x_StdPeriph_Examples\EXTI\EXTI_Example
this projectshows how to configure external interrupt lines, 3 EXTI lines (EXTI5, EXTI6 and EXTI13) when using the STM32303C-EVALare configured to generate an interrupt on each falling or rising edge.
In the interrupt routine a led connected to a specific GPIO pin is toggled.In this example:
- EXTI5 is mapped to PD5 - EXTI6 is mapped to PE6 - EXTI13 is mapped to PC13-Nesrine-
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-11-24 9:33 AM
Hello,
Did you get interrupts working? I'm also trying to use the STD Periph lib in Keil but not having much success.
Randy
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-11-24 11:25 AM
Posted on November 24, 2017 at 19:25
,
,
The code you posted was some odd register level stuff, not the Standard Peripheral Library (SPL)
Here a PB4 example in SPL. Make sure PB4 doesn't have any other connectivity on board that might interfere. Look at my accepted Best Answer:
https://community.st.com/s/feed/0D50X00009XkX90SAF
Up vote any posts that you find helpful, it shows what's working..