2020-04-22 01:44 AM
My PC runs Linux and I have two USB cables connected to my NUCLEO-H745ZI-Q board (https://www.st.com/en/evaluation-tools/nucleo-h745zi-q.html)
I have installed STM32CubeProgrammer and followed the instructions for preparing USB serial link for flashing in https://wiki.st.com/stm32mpu/wiki/STM32CubeProgrammer
When running STM32_Programmer.sh -l usb I get the following:
```
> STM32_Programmer.sh -l usb
-------------------------------------------------------------------
STM32CubeProgrammer v2.3.0
-------------------------------------------------------------------
===== DFU Interface =====
No STM32 device in DFU mode connected
```
And apparently the flash programming does not work either:
```
> STM32_Programmer.sh -c port=/dev/ttyACM1 -d m4.elf
-------------------------------------------------------------------
STM32CubeProgrammer v2.3.0
-------------------------------------------------------------------
Serial Port /dev/ttyACM1 is successfully opened.
Port configuration: parity = even, baudrate = 115200, data-bit = 8,
stop-bit = 1,0, flow-control = off
Error: Activating device: KO. Please, verify the boot mode configuration and check the serial port configuration. Reset your device then try again...
```
Now I am stuck with how to enable DFU-mode on my board.
Please advise.
2020-04-22 02:13 AM
Digging further:
According to https://www.st.com/content/ccc/resource/technical/document/application_note/b9/9b/16/3a/12/1e/40/0c/CD00167594.pdf/files/CD00167594.pdf/jcr:content/translations/en.CD00167594.pdf p. 217 "The STM32H74xxx/75xxx bootloader is activated by applying pattern10 (described in Ta b l e2: Bootloader activation patterns). "
, where pattern10 (according to Table 2) is either
"Boot(pin) = 0 and BOOT_ADD0(optionbyte) = 0x1FF0"
or
"Boot(pin) = 1 and BOOT_ADD1(optionbyte) = 0x1FF0"
Looks like Boot(pin) is referring to pin CN11.7 (BT0) on my EVK's PCB, but what is BOOT_ADD0 and BOOT_ADD1 are and how to set them remains unclear.
2020-04-22 02:25 AM
Some more information.
The ouput of lsusb on my setup:
```
> lsusb
Bus 001 Device 025: ID 0483:374e STMicroelectronics STLINK-V3
```