cancel
Showing results for 
Search instead for 
Did you mean: 

How to configure USB CDC <<FS>> on STM32H7A3? (Only HS available)

GS1
Senior III

Hi all,

I am just starting a new project with a STM32H7A3 processor and need to connect the system via USB as Device in CDC mode (Virtual COM Port).

STM32CubeMX only allows to configure HS instead of FS. What has to be done to use the USB port in FS mode? Is there a working sample code available for the H7A3 and USB CDC in FS mode? (Could not find it in the Sample section for the Nucleo H7A3 board)

Thank you for any assistance.

GS

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0