cancel
Showing results for 
Search instead for 
Did you mean: 

How can I get the embedded demonstration example for P-NUCLEO-USB002 kit?

MMevo.1
Associate II

After testing P-NUCLEO-USB002 kit with it's embedded demonstration example I try to use different example from en.STSW-STUSB010 examples- it seems like non of them support UART interface (CLI) as in P-NUCLEO-USB002 embedded demonstration example. my questions are: 1. How can I get the P-NUCLEO-USB002 embedded demonstration example? 2. Is there a way to enable UART interface (CLI) in en.STSW-STUSB010 examples? Thanks, Maor

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
SKaiba
Associate

I unfortunately have the same Problem after I flashed one of the Projects from the en.STSW-STUSB010 Library.

NBALL
ST Employee

Hello

The software package does not embed demo CLI.

If you want to add CLI into the project, UART is already setup for 'Tx' in order to output debug trace: just follow _DEBUG switch.

I put in attach file demo binary if this is just what you are looking for.

Best regards