cancel
Showing results for 
Search instead for 
Did you mean: 

hi, how to erase the previous data in SD card using erase command in stm32f103c8.

mrsmile
Associate III
 
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Imen.D
ST Employee

Hello @mrsmile​,

You'll probably want to review IAP examples within STM32CubeF1:

STM32Cube_FW_F1_Vx.x.x\Projects\STM3210C_EVAL\Applications\IAP

Please have a look at this AN3990 it may be helpful to what you expect to do, and it's applicable for SD card using.

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen

hello mam @Imen DAHMEN ,

ok mam, i'll refer this document. thank you for your response. its may be helpfull for me. once again thank you mam.

hello mam,

i'm need to erase the previous data in SD card(SPI communication) by using erase command in stm32f103c8(HAL library).

in this condition using to continuously erase the data.

uint8_t erase_cmd[6]={0x20, 0x00, 0x00, 0x00, 0x00, 0x95};

HAL_GPIO_WritePin(GPIOB, GPIO_PIN_0, GPIO_PIN_RESET);   // Chip select pin

HAL_SPI_Transmit(&hspi1, erase_cmd, sizeof(erase_cmd), HAL_MAX_DELAY);

HAL_SPI_Receive(&hspi1, &status, 1, HAL_MAX_DELAY); 

HAL_GPIO_WritePin(GPIOB, GPIO_PIN_0, GPIO_PIN_SET);.