cancel
Showing results for 
Search instead for 
Did you mean: 

Hi all, Does anybody has any idea what is "The parameter is incorrect" error. I am using nucleo f429zi board. the problem occurs when i am using ethernet with the USB. The PC can detect the virtual com port but gives error when you try to connect to it.

Mr ZEE
Associate II

If i disable the ethernet (comment the MX_LWIP_INIT function) the USB works fine. I am only using the cube MX generated code no fancy thing at all. The next thing I tried to do was to do the same thing on STM3249zi eval board but I was surprised to see that USB was working fine with the ethernet, no errors at all.

The question is that is it something to do with the hardware?

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0