cancel
Showing results for 
Search instead for 
Did you mean: 

STM32G071 disco USBPD_Analyzer

aber
Associate

Hi,

I am trying to modify the USBPD_Analyer Demonstration to use a fixed PDO definition in the usbpd_pdo_defs.h

Eventually I would like to modify it to create a source slave as it is not available in the CubeMonitor-UCPD but to begin with I am just adding the fixed sources already in the code.

I have commented out 

#define _USBPD_PWR_IF_C      in usbpd_pwr_if.c 

to use the definition of

PORT0_PDO_ListSNK[USBPD_MAX_NB_PDO]  in the usbpd_pdo_defs.h

and I have also added 

#include "usbpd_pwr_if.h" to the usbpd_pdo_defs.h

as the compiler was warning of implicit declarations of PWR_A_50MA, PWR_V_100MV etc.

Now when I compile the project I get

multiple definition of PORT0_PDO_ListSNK 

multiple definition of USBPD_NbPDO 

in usbpd_dpm_core.ousbpd_dpm_user.o, bsp_gui.o  and gui_api.o

I can see that PORT0_PDO_ListSNK is used in these file but don't understand why it thinks there are multiple definitions. 

I would be grateful if you could explain what I am doing wrong or let me know how to define a PDO definition for a source slave.

Thanks 

 

 

1 ACCEPTED SOLUTION

Accepted Solutions
FBL
ST Employee

Hi @aber 

An internal ticket is already submitted to developers to adjust include order to ensure that macro __USBPD_PWR_IF_C is defined before usbpd_pdo_defs.h is included. Check this thread as well Re: Issue with MACROs after generating code using ... - STMicroelectronics Community

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.




Best regards,
FBL

View solution in original post

1 REPLY 1
FBL
ST Employee

Hi @aber 

An internal ticket is already submitted to developers to adjust include order to ensure that macro __USBPD_PWR_IF_C is defined before usbpd_pdo_defs.h is included. Check this thread as well Re: Issue with MACROs after generating code using ... - STMicroelectronics Community

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.




Best regards,
FBL