HAL_PCDEx_PMAConfig Calculation help for Stream of YUY2 Image format.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2025-03-07 7:24 AM
Hello!
I am working on Implementing a Uncompressed YUV2 Stream through the Windows Camera Application with an STM32H5 Series Board. I am looking for an example of these values, the HAL_PCDEx_PMAConfig Values, as these are what establish the USB payload buffer to send my images through a stream2.h file found in this project (https://github.com/STMicroelectronics/x-cube-azrtos-h7/tree/main/Projects/NUCLEO-H723ZG/Applications/USBX/Ux_Device_Video/Stream) . The H5 doesn't support USB-OTG, so I have been trying to find an example of a project that is a USBX Video that uses USB FS functionality. (The linked project uses USB-OTG so instead it uses HAL_PCDEx_SetRxFiFo/SetTxFifo to establish a payload)
These values worked with the stream1.h file from that same project linked above. However I am unable to change these values for a YUV2 stream to successfully stream.
HAL_PCDEx_PMAConfig(&hpcd_USB_DRD_FS, 0x00, PCD_SNG_BUF, 0x10);
HAL_PCDEx_PMAConfig(&hpcd_USB_DRD_FS, 0x80, PCD_SNG_BUF, 0x50);
HAL_PCDEx_PMAConfig(&hpcd_USB_DRD_FS,USBD_VIDEO_EPIN_ADDR , PCD_DBL_BUF, 0x01900090);
Any guidance?
- Labels:
-
STM32H5 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2025-04-29 3:45 AM
Hi @treepreeyuh
Have you tried to generate code using CubeMX?
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.