Skip to main content
Associate
September 30, 2025
Solved

FreeRTOS Tickless mode

  • September 30, 2025
  • 1 reply
  • 344 views

Hi all,

I ran into an issue regarding FreeRTOS tickless idle mode. I wanted to share my findings and solution in case others encounter the same problem and also to ask if that's intended structure (so I am missing something) or if its not generated properly.

Background:

  • I was using SysTick as the OS kernel timebase.

  • Tickless idle was enabled (configUSE_TICKLESS_IDLE = 1).

  • I noticed that the portNVIC_SYSTICK_COUNT_FLAG_BIT was cleared unexpectedly during sleep, which caused the tickless idle implementation (vPortSuppressTicksAndSleep) to miscalculate elapsed ticks.

  • Debugging revealed that the auto-generated SysTick_Handler in cmsis_os2.c was clearing the COUNTFLAG, even in tickless mode.

The autogenerated handler looked like this:

 

 
void SysTick_Handler(void) {
 /* Clear overflow flag */
 SysTick->CTRL;

 if (xTaskGetSchedulerState() != taskSCHEDULER_NOT_STARTED) {
 xPortSysTickHandler();
 }
}
  • Reading the Cortex-M documentation shows that reading SYST_CSR clears the COUNTFLAG.

  • This means that the autogenerated handler clears COUNTFLAG before the FreeRTOS tickless idle logic can use it, breaking tickless idle functionality.

Solution:

  • The fix is to override the SysTick_Handler :

extern void xPortSysTickHandler(void);

void SysTick_Handler(void) {
#if !defined(configUSE_TICKLESS_IDLE) || (configUSE_TICKLESS_IDLE == 0)
 /* Clear overflow flag only if not using tickless idle */
 SysTick->CTRL;
#endif
 if (xTaskGetSchedulerState() != taskSCHEDULER_NOT_STARTED) {
 xPortSysTickHandler();
 }
}
 

With this override, tickless idle works properly, and COUNTFLAG is preserved for vPortSuppressTicksAndSleep.

 

Question: 
Am i supposed to be doing that overwrite? Shouldn't the tickless auto-generated code be "Ready to use"?

Thank you for your time.

 

Best answer by bmckenney

ST is apparently in the process of fixing this:

https://community.st.com/t5/stm32cubemx-mcus/cubemx-1-19-cmsis-os2-c-systick-handler-breaks-freertos-if/m-p/836854

Your fix looks more nuanced than that in the other thread.

1 reply

bmckenneyBest answer
Explorer II
September 30, 2025

ST is apparently in the process of fixing this:

https://community.st.com/t5/stm32cubemx-mcus/cubemx-1-19-cmsis-os2-c-systick-handler-breaks-freertos-if/m-p/836854

Your fix looks more nuanced than that in the other thread.

MartíAuthor
Associate
October 1, 2025

Hi bmckenney,

Thanks for sharing this post! I couldn’t find much information on this topic elsewhere, and this really helped clear things up.
Much appreciated—cheers!