Skip to main content
Associate III
September 7, 2025
Question

CubeMX 1.19 cmsis_os2.c SysTick_Handler breaks FreeRTOS if configUSE_TICKLESS_IDLE == 1

  • September 7, 2025
  • 4 replies
  • 713 views

I am having a "how did this ever work" moment. Maybe I found a (horrible) bug, or maybe I'm overlooking something.

In tickless idle mode FreeRTOS uses the COUNTFLAG in the SysTick SYST_CSR to determine if WFI exited due to the systick, and then calculates how many RTOS ticks have elapsed:

			configPRE_SLEEP_PROCESSING( xModifiableIdleTime );
			if( xModifiableIdleTime > 0 )
			{
				__asm volatile( "dsb" ::: "memory" );
				__asm volatile( "wfi" );
				__asm volatile( "isb" );
			}
			configPOST_SLEEP_PROCESSING( xExpectedIdleTime );

			/* Re-enable interrupts to allow the interrupt that brought the MCU
			out of sleep mode to execute immediately. see comments above
			__disable_interrupt() call above. */
			__asm volatile( "cpsie i" ::: "memory" );
			__asm volatile( "dsb" );
			__asm volatile( "isb" );

			/* Disable interrupts again because the clock is about to be stopped
			and interrupts that execute while the clock is stopped will increase
			any slippage between the time maintained by the RTOS and calendar
			time. */
			__asm volatile( "cpsid i" ::: "memory" );
			__asm volatile( "dsb" );
			__asm volatile( "isb" );

			/* Disable the SysTick clock without reading the
			portNVIC_SYSTICK_CTRL_REG register to ensure the
			portNVIC_SYSTICK_COUNT_FLAG_BIT is not cleared if it is set. Again,
			the time the SysTick is stopped for is accounted for as best it can
			be, but using the tickless mode will inevitably result in some tiny
			drift of the time maintained by the kernel with respect to calendar
			time*/
			portNVIC_SYSTICK_CTRL_REG = ( portNVIC_SYSTICK_CLK_BIT | portNVIC_SYSTICK_INT_BIT );

			/* Determine if the SysTick clock has already counted to zero and
			been set back to the current reload value (the reload back being
			correct for the entire expected idle time) or if the SysTick is yet
			to count to zero (in which case an interrupt other than the SysTick
			must have brought the system out of sleep mode). */
			if( ( portNVIC_SYSTICK_CTRL_REG & portNVIC_SYSTICK_COUNT_FLAG_BIT ) != 0 ) <<<<<< Checks the count flag here

 

However, notice that FreeRTOS briefly enables and disables interrupts to allow whatever pended interrupt caused wfi to exit to be serviced.  Usually this will be the systick interrupt.

cmsis_os2.c provides a "helpful" wrapper for the systick interrupt - and the very first thing it does is to clear the systick count flag bit:

#if (USE_CUSTOM_SYSTICK_HANDLER_IMPLEMENTATION == 0)
void SysTick_Handler (void) {
 /* Clear overflow flag */
 SysTick->CTRL; <<<<<<<<<<<<<<<<< this is not good

 if (xTaskGetSchedulerState() != taskSCHEDULER_NOT_STARTED) {
 /* Call tick handler */
 xPortSysTickHandler();
 }
}
#endif

As far as I can tell this means that the default code generated by CubeMX for the case of configUSE_TICKLESS_IDLE == 1 cannot work because as soon as FreeRTOS finds the conditions where it can use tickless idle then the FreeRTOS tick will stop incrementing.  This is because when the systick wakes the processor from wfi  FreeRTOS will think that a different interrupt woke the processor and if you follow that code path, and realizing that the systick counter has just rolled over (since it caused the wake) FreeRTOS calculates that only a fraction of a tick has elapsed.

Like I said, this is so fundamental that this is causing me a "how can this have ever worked or am I missing something blindingly obvious" moment.

Thanks

 

4 replies

Ghofrane GSOURI
ST Technical Moderator
September 8, 2025

Hello @sdtbb 

Could you please provide your .ioc file? This will allow me to review your configuration in detail and better understand the issue you are experiencing.

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
sdtbbAuthor
Associate III
September 8, 2025

Hi @Ghofrane GSOURI 

Please find attached. 

Thanks

Sean

Ghofrane GSOURI
ST Technical Moderator
September 9, 2025

Hello @sdtbb 

Thank you very much for your contribution.

The issue has been escalated to the development team.
The internal ticket number is 217124.

I will keep you updated with any progress.

THX

Ghofrane

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
sdtbbAuthor
Associate III
September 9, 2025

Thank you for the support. I should add that commenting out this line in SysTick_Handler() in cmsis_os2.c fixes the problem with tickless idle.

#if (USE_CUSTOM_SYSTICK_HANDLER_IMPLEMENTATION == 0)
void SysTick_Handler (void) {
 /* Clear overflow flag */
 //SysTick->CTRL; <<<<< Commented out - now FreeRTOS tickless idle works correctly

 if (xTaskGetSchedulerState() != taskSCHEDULER_NOT_STARTED) {
 /* Call tick handler */
 xPortSysTickHandler();
 }
}
#endif