Skip to main content
Dilbert K
Associate III
April 22, 2024
Question

FreeRTOS_MPU

  • April 22, 2024
  • 5 replies
  • 2846 views

STM32Cube_FW_L4_V1.18.0\Projects\NUCLEO-L476RG\Applications\FreeRTOS\FreeRTOS_MPU

I am trying to debug the usage of FreeRTOS_MPU using the NUCLEO-L476RG board.

But the code failed at HAL_Init() - 

if (HAL_InitTick(TICK_INT_PRIORITY) != HAL_OK)

{

status = HAL_ERROR;

}

 

Anyone has any idea ?

 

p.s.

I loaded up the other FreeRTOS example and works OK.

STM32Cube_FW_L4_V1.18.0\Projects\NUCLEO-L476RG\Applications\FreeRTOS\FreeRTOS_ThreadCreation

5 replies

Pavel A.
April 22, 2024

With FreeRTOS, your HAL timer is one of the STM32 TIM timers rather than systick. Which timer is it? Try to trace into HAL_InitTick and see where it fails.

 

Dilbert K
Dilbert KAuthor
Associate III
April 25, 2024

I have located the issue but have no idea how to fix the STM32Cube_FW code

The global variables are not initialized in "stm32l4xx_hal.c" of project "NUCLEO-L476RG\Applications\FreeRTOS\FreeRTOS_MPU"

 

 

/** @defgroup HAL_Exported_Variables HAL Exported Variables
 * @{
 */
__IO uint32_t uwTick;
uint32_t uwTickPrio = (1UL << __NVIC_PRIO_BITS); /* Invalid priority */
HAL_TickFreqTypeDef uwTickFreq = HAL_TICK_FREQ_DEFAULT; /* 1KHz */

 

 uwTickPrio and uwTickFreq are zero.

 

In other project "NUCLEO-L476RG\Applications\FreeRTOS\FreeRTOS_ThreadCreation",

both variables are initialized correctly.

Pavel A.
April 25, 2024

> uwTickPrio and uwTickFreq are zero.

This hints to a problem with RAM allocation. Like, static data collides with thread stacks, or gets clobbered by something else, or just sits in a wrong place.

Dilbert K
Dilbert KAuthor
Associate III
April 25, 2024

With more debug...  here is the result...

1. "STM32Cube_FW_L4_V1.18.0\Projects\NUCLEO-L476RG\Applications\FreeRTOS\FreeRTOS_MPU"

- Using STM32CubeIDE_1.15.0 --> does NOT work

 

2. "STM32Cube_FW_L4_V1.17.0\Projects\NUCLEO-L476RG\Applications\FreeRTOS\FreeRTOS_MPU"

- Using SystemWorkbench (AC6) --> working OK

 

Hope not the issue in the new STM32CubeIDE_1.15.0.  As I want to switch over to the new STM supported tools.

 

Pavel A.
April 27, 2024
Dilbert K
Dilbert KAuthor
Associate III
April 28, 2024

Thanks for the extra info.

However, the "STM32Cube_FW_L4_V1.18.0" suppose to support stm32cubeide as all the projects already had converted by STM engineers.

If this is the case, even if I follow the instruction, would the result be the same as the release ??

Pavel A.
April 28, 2024

 the projects already had converted by STM engineers.

Then unfortunately it's a bug. It looks like regression testing is missing there for CubeIDE and library package updates.