Freertos and HAL external interrupts
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-11-09 6:39 AM
Hello,
I'm using stm32l496.
i'm trying to control LEDs with pwm through freeRTOS and using external Interrupts (gpio buttons)
i have some questions :
i have some tasks looping while(1) to detect my input GPIO and launch PWM timer :
void TASK(void)
{
while(1)
{if(HAL_GPIO_ReadPin(GPIOD, GPIO_PIN_1) == GPIO_PIN_SET)
{HAL_TIM_PWM_Start(&htim16, TIM_CHANNEL_1);
while(HAL_GPIO_ReadPin(GPIOD, GPIO_PIN_1) == GPIO_PIN_SET)
{ __HAL_TIM_SET_COMPARE(&htim16, TIM_CHANNEL_1, 2000); osDelay(200);;__HAL_TIM_SET_COMPARE(&htim16, TIM_CHANNEL_1, 0);
osDelay(200);}}
}
i'm using 10 tasks like this to activate leds on demand.
Sometimes, the PWM led doesn't start though.
i guess there is better way using External Interrupts right ?
When i use external input EXTI0_IRQHandler() to do same task
it crashes freertos.
when i use the
EXTI0_IRQHandler()
without freertos activated, in another project, it works.How to correctly use external interrupts with freertos ? or correctly launch my timers within tasks ?
I guess my program is too much time consuming and it lags...
Thank you
#gpio-interrupt #pwm #freertos+hal- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-11-09 8:14 PM
Hi, rolly!
You should use TaskNotification
()
or TaskNotificationFromISR(), in the terminology of freeRTOS. (or osSignalSet if you use CMSIS OS API).Please have a look at following document.
,Chapter 9.Also, if you are porting freeRTOS to CMSIS-OS, you may also take a look at some ST-Examples like
'Your Cube Folders'\STM32Cube_FW_L4_V1.8.0\Projects\STM32L496ZG-Nucleo\Applications\FreeRTOS\FreeRTOS_SignalFromISR
Signals or TaskNotify is the most efficient way to trigger a task, without the need of an intermediate communication object!
Good Luck!
.Zt
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-11-10 2:50 AM
Thank you ZhiTai !
I've check that Application folder.
actually i'm starting my task like this :
xTaskCreate(TASK
, 'IRQPwmLedShow1', configMINIMAL_STACK_SIZE, //AR_GAUCHE NULL, tskIDLE_PRIORITY + 1, &xLedIRQPwmHandler1);....
while(1)
{
vTaskResume(xLedPwmHandler1);
...
}
When you mention 'TaskNotification()
or TaskNotificationFromISR()'
you mean xTaskNotifyGive() xTaskNotify() and vTaskNotifyGiveFromISR() ?
External hardware interrupt (
EXTI0_IRQHandler) is same as software ISR ?
I just want to start a task when i push a button.
Thank you for your help
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-11-10 6:40 PM
Suppose you port your freeRTOS successfully.
Try the following codes, pretty mush the same as the example in chapter 9 of the ref book I gave you.
/* The tasks to be created. */
static void vHandlerTask( void *pvParameters );
/* Stores the handle of the task to which interrupt processing is deferred. */
static TaskHandle_t xTaskHandler = NULL;
int main(void)
{
/*your initialization codes*/
/* Create the 'handler' task, which is the task to which interrupt
processing is deferred, and so is the task that will be synchronized
with the interrupt.*/
xTaskCreate( vHandlerTask, 'Handler', 128, NULL, 3, &xTaskHandler );
/* Start the scheduler so the created tasks start executing. */
vTaskStartScheduler();
}
static void vHandlerTask( void *pvParameters )
{
uint32_t ulNotifyValue;
for(;;)
{
/* Wait to receive a notification sent directly to this task from the interrupt handler. */
ulNotifyValue = ulTaskNotifyTake(pdTRUE, 0xFFFFFFFF);
if(ulNotifyValue != 0)
{
/*Your task job here*/
BSP_LED_Toggle(LED1);
}
}
}
/*Your general GPIO_EXTI Callbacks here*/
void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin)
{
/* The xHigherPriorityTaskWoken parameter must be initialized to pdFALSE */
BaseType_t xHigherPriorityTaskWoken;
xHigherPriorityTaskWoken = pdFALSE;
/* your user button callback here*/
if(GPIO_Pin == USER_BTN_PIN)
{
/* Send the notification directly to the task handler*/
vTaskNotifyGiveFromISR( xTaskHandler, &xHigherPriorityTaskWoken );/*If xHigherPriorityTaskWoken was set to pdTRUE inside vTaskNotifyGiveFromISR()
then calling portYIELD_FROM_ISR() will request a context switch. */ portYIELD_FROM_ISR( xHigherPriorityTaskWoken );}
}
It works in my Discovery F412.
You may also use oscilloscope to check the time between the button push and the trigger of your task.
Good Luck, rolly!
.Zt
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-12-25 9:10 AM
Hello,
I have the same issue, and I tried the above suggestion, but nothing change.
I am not sure why freeRTOS fail to receive interrupt(?).
Any ideas ?
Ran