2023-03-13 7:54 AM
I would like to use NUCLEO-G071RB and X-NUCLEO-DRP1M1 to Source,UFP my USB devices
When the USB device side is set as Source, the role of data is DFP.
I used the DR SWAP command to change from DFP to UFP.
But there was no sample code in x-cube-tcpp_v4.0.0.
I thought the following APIs would be applicable
-- USBPD_StatusTypeDef USBPD_DPM_EvaluateDataRoleSwap(uint8_t PortNum)
How should I use it?
Best Regards
2023-03-29 6:58 AM
Hello @forst
The below function can be used :
USBPD_StatusTypeDef USBPD_DPM_RequestDataRoleSwap(uint8_t PortNum)
{
USBPD_StatusTypeDef _status = USBPD_PE_Request_CtrlMessage(PortNum, USBPD_CONTROLMSG_DR_SWAP, USBPD_SOPTYPE_SOP);
DPM_USER_ERROR_TRACE(PortNum, _status, "DRS not accepted by the stack");
return _status;
}A similar use case (automatic power role swap) is described in our wiki.
Does it help ?
And a data role swap call example is available in the STM32G0 discovery analyser demonstration firmware here on github.
If you have a look on the wiki, have a look also at the debug tool, and the stack user manual.
Regards,
Nicolas